9DoF Razor IMU M0 Hookup Guide

≡ Pages
Contributors: jimblom

Resources and Going Further

Our GitHub repostiory for the SparkFun 9DoF Razor IMU M0, includes all of our hardware and firmware design files. You can check out the board's schematic, Eagle PCB layout, or the example firmware over there.

For more on the 9DoF Razor IMU's MPU-9250, here are a handful of resources worth checking out:

There are plenty of tutorials left, if you need some project inspiration. Check out some of these related tutorials:

Dungeons and Dragons Dice Gauntlet

A playful, geeky tutorial for a leather bracer that uses a LilyPad Arduino, LilyPad accelerometer, and seven segment display to roll virtual 4, 6, 8, 10, 12, 20, and 100 side dice for gaming.

MicroView Digital Compass

Build a portable digital compass using the SparkFun MicroView and the MAG3110 Magnetometer Breakout.

MPL3115A2 Pressure Sensor Hookup Guide

Getting started with the MPL3115A2 Pressure Sensor.

Are You Okay? Widget

Use an Electric Imp and accelerometer to create an "Are You OK" widget. A cozy piece of technology your friend or loved one can nudge to let you know they're OK from half-a-world away.

Or check out this blog post for ideas: