GNSS Timing Breakout - ZED-F9T (Qwiic) Hookup Guide

Pages
Contributors: Nate, El Duderino

Introduction

Introducing the SparkFun GNSS Timing Breakout - ZED-F9T (Qwiic), a unique entry into SparkFun's GNSS catalog featuring the ZED-F9T GNSS receiver from u-blox. The ZED-F9T provides up to 5 nanosecond timing accuracy under clear skies with no external GNSS correction making it perfect for applications where timing accuracy is imperative. Need an extremely accurate time reference to maximize the efficiency of your IoT network of 5G devices? The GNSS Timing Breakout - ZED-F9T could be the perfect solution.

SparkFun GNSS Timing Breakout - ZED-F9T (Qwiic)

GPS-18774
$309.95

This breakout shares a similar design as the SparkFun GPS-RTK-SMA Breakout to create a small but comprehensive development tool for ZED-F9T. The design includes a USB-C connector for primary power and communication, two Qwiic connectors for communicating over I2C using the SparkFun Qwiic system, three SMA connectors for the antenna and timing pulse signals as well as a host of PTH pins allowing direct interaction with most of the ZED-F9T's pinout.

Required Materials

You will need the following materials along with the SparkFun GNSS Timing Breakout - ZED-F9T (Qwiic) to follow along with this tutorial.

GNSS Antenna

The ZED-F9T is a dual receiving GNSS receiver which means it can receive both L1 and L2 GNSS frequencies. To enable this, you will need an appropriate antenna such as those listed below:

GNSS Multi-Band L1/L2/L5 Surveying Antenna - TNC (SPK6618H)

GPS-21801
$169.95

GNSS L1/L2 Multi-Band Magnetic Mount Antenna - 5m (SMA)

GPS-15192
$109.95

MagmaX2 Active Multiband GNSS Magnetic Mount Antenna - AA.200

GPS-17108
Retired

GNSS Multi-Band L1/L2 Helical Antenna (SMA) BT-560

GPS-17383
Retired

A low cost GNSS antenna will work and provide a basic fix but the advanced timing and positional accuracy features of the ZED-F9T will not be available without L2 support.

USB Cable

Basic use of the ZED-F9T either through a serial terminal or u-blox's u-center application needs a USB-C cable to connect the board to your computer:

Reversible USB A to C Cable - 0.3m

CAB-15426
$5.50

Reversible USB A to C Cable - 0.8m

CAB-15425
$6.50

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

Reversible USB A to C Cable - 2m

CAB-15424
$10.50

Arduino Examples Materials

For those who want to use the breakout board with the SparkFun u-blox GNSS Arduino Library, you'll need an Arduino microcontroller, Qwiic cable and USB-C cable to get started. We found the ESP32 works as a great transmitting option when creating a network of GNSS devices receiving time correction data from a ZED-F9T configured to act as a base station:

SparkFun Qwiic Cable Kit

KIT-15081
$12.95

SparkFun Thing Plus - ESP32 WROOM (Micro-B)

WRL-15663
$24.95

SparkFun Thing Plus - ESP32-S2 WROOM

WRL-17743
$24.50

Qwiic Cable - 100mm

PRT-14427
Retired

SparkFun u-blox library examples

The SparkFun u-blox GNSS Arduino Library has a tremendous number of examples and features to demonstrate the power of our GNSS receivers. For the ZED-F9T specifically, be sure to view the Time Pulse examples. These will show you how to configure the time pulse settings for the two time pulse outputs.

While configuring the ZED-F9T over Qwiic from a microcontroller is pretty easy, many applications for timing require a set it and forget it mentality. Consider using u-center from u-blox to configure your ZED-F9T over USB and then saving the configuration to BBR (battery backed RAM) so that the module comes on with the same settings at the next power on.

Recommended Reading

Before getting started with the GNSS Timing Breakout you may want to read through these tutorials if you are not familiar with the concepts covered in them:

GPS Basics

The Global Positioning System (GPS) is an engineering marvel that we all have access to for a relatively low cost and no subscription fee. With the correct hardware and minimal effort, you can determine your position and time almost anywhere on the globe.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Basic Hookup Guide

Get connected quickly with this Serial to USB adapter.

Getting Started with U-Center for u-blox

Learn the tips and tricks to use the u-blox software tool to configure your GPS receiver.