GNSS Timing Breakout - ZED-F9T (Qwiic) Hookup Guide
Contributors:
Nate,
El Duderino
Resources and Going Further
That's a wrap for this tutorial. For more information about the SparkFun GNSS Timing Breakout - ZED-F9T (Qwiic), check out the following resources:
- Schematic (PDF)
- Eagle Files (ZIP)
- Board Dimensions (PNG)
- Datasheet (PDF) (ZED-F9T)
- Integration Manual (PDF) (ZED-F9T)
- Interface Description Reference (PDF) (ZED-F9T)
- Differential Timing Setup AppNote (PDF) (ZED-F9T)
- u-center Software
- SparkFun u-blox GNSS Arduino Library
- GitHub Hardware Repository
For more information on setting up a GNSS Timing Breakout - ZED-F9T as a time base station and broadcasting RTCM data, head over to these tutorials:
- What is GPS RTK? - What is RTCM
- Setting Up a Rover Base RTK System - Setting Up a Temporary Base
- How to Build a DIY GNSS Reference Station:
Looking for inspiration for your next GNSS project? The tutorials below may help:
SparkFun GPS Breakout - XA1110 (Qwiic) Hookup Guide
Figure out where in the world you are with the Qwiic SparkFun GPS Breakout - XA1110.
Basic Autonomous Kit for Sphero RVR Assembly Guide
Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!
SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide
The u-blox ZED-F9R is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino and Python so that you can start reading the output!
MicroMod GNSS Carrier Board (ZED-F9P) Hookup Guide
Easily switch between Processor Boards using the MicroMod ecosystem and get precision down to the diameter of a dime with the ZED-F9P from u-blox using the MicroMod GNSS Carrier Board!