MicroMod WiFi Function Board - DA16200 Hookup Guide

≡ Pages
Contributors: Ell C

Introduction

Want to add all the IoT functionality of the DA16200 to the adaptability of the MicroMod system? Then you're in luck! The SparkFun MicroMod DA16200 Function Board adds a fully integrated WiFi module with a 40MHz crystal oscillator, 32.768KHz RTC clock, RF Lumped RF filter, 4MB flash memory, and an on-board chip antenna to any MicroMod project. With the addition of JTAG connectors for deep dive programming, you've got everything you need to get your MicroMod setup ready for your next IoT project.

SparkFun MicroMod WiFi Function Board - DA16200

WRL-18594
Retired

Required Materials

To follow along with this tutorial, you will need the following materials at a minimum. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Reversible USB A to C Cable - 2m

CAB-15424
$10.50

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

SparkFun MicroMod WiFi Function Board - DA16200

WRL-18594
Retired

MicroMod Main Board

To hold the processor board and function board, you will need one Main board. Depending on your application, you may choose to have one or two additional function boards.

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

SparkFun MicroMod Main Board - Double

DEV-18576
Retired

MicroMod Processor Board

There are a variety of MicroMod Processor Boards available to choose from.

SparkFun MicroMod Teensy Processor

DEV-16402
$24.95

SparkFun MicroMod Teensy Processor with Copy Protection

DEV-18771
$29.95

SparkFun MicroMod mikroBUS Starter Kit

KIT-19935
$79.95 $59.95

SparkFun Arduino IoT Weather Station

KIT-22636
$129.95

Tools

You will need a screw driver to secure the Processor and Function boards.

SparkFun Mini Screwdriver

TOL-09146
$1.50

MicroMod Screwdriver

TOL-19012
$0.75

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

MicroMod Artemis Processor Board Hookup Guide

Get started with the Artemis MicroMod Processor Board in this tutorial!

Designing with MicroMod

This tutorial will walk you through the specs of the MicroMod processor and carrier board as well as the basics of incorporating the MicroMod form factor into your own PCB designs!

Hardware Overview

DA16200

The MicroMod WiFi Function Board includes the DA16200 module from Dialog with AT command firmware. This chip is a fully integrated Wi-Fi® module with ultra-low power consumption, 40 MHz crystal oscillator, 32.768 KHz RTC clock, RF Lumped RF filter, 4 M-byte flash memory, and an onboard chip antenna. For more information, refer to the datasheet.

Wifi module is highlighted

Power

To power the board, you will need to apply power to a SparkFun Main Board; either a Single or a Double. Power applied will connect to the Function Board's VIN pin, which will be regulated down for the rest of the board with the AP2112 3.3V/600mA voltage regulator.

USB C of the Main board with USBC cable plugged in is highlighted

AP2112

Operating voltage for the DA16200 is 3.3 V. The AP2112 can handle a voltage range of 2.5-6V with a 600mA output and ensures appropriate voltage to the WiFi unit.

Voltage regulator is highlighted

CH340

The board is populated with the CH340E USB-to-Serial converter to update firmware on the DA16200 through its USB Type C connector. You will need a Main Board and a second USB cable to update the firmware.

CH340 and USB C are highlighted on the function board

Reset Button

The reset button allows users to reset the program running on the Dialog module without unplugging the board.

Factory Reset Button is highlighted

WPS Button

The Wi-Fi Protected Setup Button allows you to easily and quickly connect to a WiFi network.

WPS Button is highlighted

EEPROM

The board includes an I2C EEPROM. To enable writing to the EEPROM, pull WP low, either through the EEPROM_WP pin or by closing JP3.

EEProm is highlighted

JTAG

An unpopulated JTAG footprint is available for more advanced users who need breakpoint level debugging. We recommend checking out our JTAG section for the compatible male header and a compatible JTAG programmer and debugger.

JTAG pins are highlighted

LED

There is only one LED available which is the Power LED. The LED lights up to indicate availability for the DA16200 from the 3.3V voltage regulator. You can disable it by cutting the jumper on the back of the board (see Jumpers below).

Power LED is just below the WiFi module on the right side of the board

Jumpers

The following jumpers are included to configure the board.

  • PWR - By default, the jumper with the label PWR is closed. This jumper connects the 3.3V line and LED. Cutting this jumper will disable the LED.

Power LED Jumper is on the back of the board on the opposite side from the M2 connector

  • I2C Pull-up Resistors - By default, this three way jumper labeled I2C is closed and connects two pull-up resistors to the I2C data lines. If you have many devices on your I2C data lines, then you may consider cutting these two jumpers.

I2C jumper is on the front of the board to the left of the WPS button

  • WP - By default, write protect for the EEPROM is on. To disable write protection, close this jumper.

Write protect jumper is on the back of the board just next to the M2 Connector

Hardware Pinout

The M.2 connector on the MicroMod WiFi Function Board - DA16200 is routed according to the pinout chart below:

Highlighted function board M.2 connector

Depending on your window size, you may need to use the horizontal scroll bar at the bottom of the table to view the additional pin functions. Note that the M.2 connector pins on opposing sides are offset from each other as indicated by the bottom pins where it says (Not Connected)*. There is no connection to pins that have a "-" under the primary function.

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Description Function Bottom
Pin
   Top   
Pin
Function Description
(Not Connected) 75 GND
- 74 73 3.3V Power Supply: 3.3-6V
- 72 71 Power EN Power Supply: 3.3-6V
- 70 69 -
- 66 65 -
- 64 63 -
- 62 61 -
- 60 59 -
- 58 57 RTC_WAKE1 This pin is an input pin for receiving an external event signal from an external device like a sensor. The RTC block detects an external event signal via this pin and wakes up DA16200 from Sleep mode 2 or Sleep mode 3.
- 56 55 RTC_WAKE2 This pin is an input pin for receiving an external event signal from an external device like a sensor. The RTC block detects an external event signal via this pin and wakes up DA16200 from Sleep mode 2 or Sleep mode 3.
- 54 53 RTC_PWR_KEY Enable to kick off a predefined power-up sequence and eventually all the necessary power is supplied to all the sub-blocks including the main digital block in DA16200. When disabled, all blocks are powered off and this mode is defined as Sleep mode 1.
- 52 51 GPIOA11
- 50 49 CS
- 48 47 GPIOA10
- 46 45 GND
- 44 43 -
- 42 41 -
Controls the write protection pin for the EEPROM. Pull low to enable. EEPROM_WP 40 39 GND
- 38 37 -
Controls EEPROM's I2C address configuration. EEPROM_A0 36 35 -
Controls EEPROM's I2C address configuration. EEPROM_A1 34 33 GND
Controls EEPROM's I2C address configuration. EEPROM_A2 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 -
- 22 21 I2C_SCL I2C - Clock signal for EEPROM
- 20 19 I2C_SDA I2C - Data signal for EEPROM
- 18 17 -
- 16 15 U1_RXI
- 14 13 U1_TXO
- 12 11 -
- 10 9 -
- 8 7 CIPO
- 6 5 COPI
- 4 3 SCK
- 2 1 GND

Board Dimensions

The board uses the standard MicroMod Function Board size which measures about 1.50"x2.56".

Board Dimensions

Hardware Hookup

Adding a Processor Board to the Main Board

Align the top key of the MicroMod Artemis Processor Board to the Processor screw terminal of your Main Board and angle the board into the socket. Insert the board at an angle into the M.2 connector.

Note: There is no way to insert the processor backward since the key prevents it from mating with the M.2 connector and as an extra safeguard to prevent inserting a processor that matches the key, the mounting screw is offset so you will not be able to secure an improperly connected processor board.

The Processor Board will stick up at an angle, as seen here:

Main board with Processor Board sticking up at an angle

Once the board is in the socket, gently push the MicroMod Processor Board down and tighten the screw with a Phillip's head.

Main board with Processor Board screwed in

Adding a Function Board to the Main Board

As with the Processor Board, align the top key of the MicroMod WiFi Function Board to the screw terminal of your Main Board on the Function Board side and angle the board into the socket. Insert the board at an angle into the M.2 connector.

Main board with Function Board sticking up at an angle

Once the board is in the socket, gently push the MicroMod Function Board down and tighten the screws with a Phillip's head.

Main board with Function Board screwed in

Once both boards are secure, your assembled MicroMod system should look similar to the image below!

Assembled main board with both processor and function boards securely fastened

DA16200 Firmware Update

To update the firmware you will need to connect the USB C cable to the MicroMod WiFi Function Board (DA16200) to a computer's COM port. An additional Main Board with a second USB C cable is also needed to power the Main Board and MicroMod WiFi Function Board.

USBC outlet on function board

Software Installation

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

Arduino Board Definitions

We'll assume that you installed the necessary board files for your Processor Board. In this case, we used the MicroMod Artemis Processor Board.

MicroMod Artemis Processor Board Hookup Guide

October 21, 2020
Get started with the Artemis MicroMod Processor Board in this tutorial!

CH340 Driver

You may need to install CH340 driver for the USB-to-serial converter. Check out our section on "How to Install CH340 Drivers" for help with the installation.

Note: If applicable, make sure you are using the proper driver files for your CPU architecture. This is usually indicated by a folder or file name with "x86" for 32-bit processors or "x64" for 64-bit processors.

Main Board Example - Pin Connection Table

For the following examples, we are using the Artemis Processor Board. For DA16200 specific pins, here is the mapping to use in Arduino sketches:

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Board
Pin Name
I/O
Direction
Main Board's
Processor Pin
Slot 0 Slot 1
VCC Input -
3.3V Input -
GND - -
RTC_WAKE1 Input G2 G7
RTC_WAKE2 Output G1 G6
RTC_PWR_KEY Input G0 G5
GPIOA11 PWM0 PWM1
CS CS0 CS1
GPIOA10 D0 D1

Example 1: Basic Connection

Copy and paste the code below into a fresh Arduino sketch.

language:c
/******************************************************************************
  Example_01 Basic Connection

  Connect to the DA16200 Module
  Print help commands

  Development environment specifics:
  IDE: Arduino 1.8.13
  Hardware Platform: MicroMod Artemis Processor, Single MicroMod Main Board

  Hardware Connections:
  Connect the MicroMod Processor Board to the Processor M2 Connector of the Main Board
  Connect the MicroMod DA16200 Function Board to the Function M2 Connector of the Main Board

  G0      --> RTC_PWR_KEY
  4       --> PWR_EN
  3.3V    --> 3.3V
  GND     --> GND

  This program is distributed in the hope that it will be useful,
  but WITHOUT ANY WARRANTY; without even the implied warranty of
  MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
  GNU General Public License for more details.

  You should have received a copy of the GNU General Public License
  along with this program.  If not, see <http://www.gnu.org/licenses/>.
******************************************************************************/    
#define PWR_EN 4
#define RTC_PWR_KEY G0

void setup() {
  pinMode(PWR_EN,OUTPUT);
  digitalWrite(PWR_EN,LOW);

  pinMode(RTC_PWR_KEY,OUTPUT);
  digitalWrite(RTC_PWR_KEY,LOW);

  Serial.begin(115200);
  Serial1.begin(115200); 

  while(!Serial){

  }
  delay(1000);



  //Enable DA16200 Module RTC power block
  pinMode(PWR_EN,OUTPUT);
  digitalWrite(PWR_EN,LOW);

  pinMode(RTC_PWR_KEY,OUTPUT);
  digitalWrite(RTC_PWR_KEY,LOW);

  Serial.println("DA16200 AT Command example sending/receiving commands\n");
  while(!Serial){

  }

  pinMode(PWR_EN,INPUT);

  pinMode(RTC_PWR_KEY,OUTPUT);
  digitalWrite(RTC_PWR_KEY,HIGH);

  delay(2000);


  //Listen for ready message ("+INIT:DONE")
  byte count = 0;
  String msg = "";

  while(count<20)
  {
    delay(100);
    while(Serial1.available())
    {
      msg += char(Serial1.read());
    }
    if(msg.length() > 5) break;
    count++;
    delay(100);
  }
  msg = msg.substring(3,msg.length());

  if(msg.length()>5)
  {
    Serial.println("Expecting: \"INIT:DONE,(0 or 1)");
    Serial.println("Received: " + msg);
  }
  else
  {
    Serial.println("Failed to receive initialization message\n");

    Serial.println("Make sure the baud rate for Serial1 matches the baud rate\n" \
                   "saved to the DA16200. You can also perform a factory reset by\n" \
                   "pressing and holding the GPIOA7 button for ~5s, which will\n" \
                   "reset the baud rate back to 115200");
  }
    Serial.println("\nTry entering \"?\" or \"help\" to print out the list of AT commands\n" \
                 "\nIf the received text is unreadable, try changing the baud rate to\n" \
                 "9600 with the command \"ATB=9600\" in the terminal. Next, update the\n" \
                 "example code by setting Serial1 to 9600 baud and trying again.\n");
}

void loop() {
    while(Serial.available())
    {
      Serial1.print(char(Serial.read()));
    }

    while(Serial1.available())
    {
      Serial.print(char(Serial1.read()));
    }
}

Set your Board and Serial Port, and then upload the sketch to your Arduino. Then open the serial monitor. Make sure your baud rate is set to 9600. You'll begin to see output.

Basic connection just makes sure you get a response from the DA16200 module

Example 2: Connecting to WiFi

Let's check out the WiFi with a simple example to grab the time.

Copy and paste the code below into a fresh Arduino sketch.

language:c
/******************************************************************************
  Example_02 WiFi Communcation

  Connect WiFi using the provided network credentials
  Talk to NTP server to set the current date/time
  Update the time to the correct time zone
  Print the current time approx. once every second

  Development environment specifics:
  IDE: Arduino 1.8.13
  Hardware Platform: MicroMod Artemis Processor, Single MicroMod Main Board

  Hardware Connections:
  Connect the MicroMod Processor Board to the Processor M2 Connector of the Main Board
  Connect the MicroMod DA16200 Function Board to the Function M2 Connector of the Main Board

  G0      --> RTC_PWR_KEY
  4       --> PWR_EN
  3.3V    --> 3.3V
  GND     --> GND

  This program is distributed in the hope that it will be useful,
  but WITHOUT ANY WARRANTY; without even the implied warranty of
  MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
  GNU General Public License for more details.

  You should have received a copy of the GNU General Public License
  along with this program.  If not, see <http://www.gnu.org/licenses/>.
******************************************************************************/
#define PWR_EN 4
#define RTC_PWR_KEY G0

String wifiSSID = "SSID";
String wifiPass = "PASSWORD";

int timezoneOffset = 0; //The hours offset from UTC (Mountain time is -6 for daylight savings, and -7 for standard)

void setup() {
  Serial.begin(115200);
  Serial1.begin(115200); 

  //Enable DA16200 Module RTC power block
  pinMode(RTC_PWR_KEY,OUTPUT);
  digitalWrite(RTC_PWR_KEY,HIGH);

  Serial.println("DA16200 AT Command Example: Connecting to WiFi\n");

  //Listen for ready message ("+INIT:DONE")
  byte count = 0;
  String msg = "";
  while(count<20)
  {
    while(Serial1.available())
    {
      msg += char(Serial1.read());
    }
    if(msg.length() > 5) break;
    count++;
    delay(100);
  }
  msg = msg.substring(3,msg.length()); //Remove NULL,CR,LF characters from response

  if(msg.length()>5)
  {
    Serial.println("Expecting: \"INIT:DONE,(0 or 1)");
    Serial.println("Received: " + msg);
  }
  else
  {
    Serial.println("Failed to receive initialization message.\n" \
                   "Make sure you're using the correct baud rate.\n");
    while(1);
  }

  //Configure module for STA mode
  Serial.println("Sending:AT+WFMODE=0");
  Serial1.println("AT+WFMODE=0");

  //Wait for "OK" response
  while(1)
  {
    msg = "";
    while(Serial1.available())
    {
      msg += char(Serial1.read());
      delay(1);
    }
    Serial.print(msg);
    if(msg.length() > 1) break;
  }

  //Apply a software reset to finish changing the mode
  Serial.println("Sending:AT+RESTART");
  Serial1.println("AT+RESTART");

  //Wait for "OK" response
  while(1)
  {
    msg = "";
    while(Serial1.available())
    {
      msg += char(Serial1.read());
      delay(1);
    }
    Serial.print(msg);
    if(msg.length() > 1) break;
  }

  //Listen for ready message ("+INIT:DONE") after the reset is finished
  count = 0;
  msg = "";
  while(count<20)
  {
    while(Serial1.available())
    {
      msg += char(Serial1.read());
    }
    if(msg.length() > 5) break;
    count++;
    delay(100);
  }

  Serial.println(count);
  Serial.println(msg);
  msg = msg.substring(3,msg.length()); //Remove NULL,CR,LF characters from response

  if(msg.length()>5)
  {
    Serial.println("Expecting: \"INIT:DONE,(0 or 1)");
    Serial.println("Received: " + msg);
  }
  else
  {
    Serial.println("Failed to receive initialization message.\n" \
                   "Continuing anyway...\n");
  }

  //Connect to WiFi using the provided credentials
  Serial.println("Sending:AT+WFJAPA=" + wifiSSID + "," + wifiPass);
  Serial1.println("AT+WFJAPA=" + wifiSSID + "," + wifiPass);

  Serial.println("Waiting for connection response...");
  while(1)
  {
    msg = "";
    while(Serial1.available())
    {
      msg += char(Serial1.read());
      delay(1);
    }

    if(msg.length() > 10) 
    {
      Serial.print("Response:");
      Serial.println(msg);
      break;
    }
  }

  msg = msg.substring(3,msg.length()); //Remove NULL,CR,LF characters from response

  //If connection to AP is successful, response will be WFJAP:1,SSID,IP_ADDRESS, or WJAP:0 if failed
  if(msg.startsWith("WFJAP:1"))
  {
      //Talk to NTP server to get the current time, along with how often to get time sync
      Serial.println("Sending:AT+NWSNTP=1,pool.ntp.org,86400");
      Serial1.println("AT+NWSNTP=1,pool.ntp.org,86400");

      //Wait for "OK" response
      while(1)
      {
        String msg = "";
        while(Serial1.available())
        {
          msg += char(Serial1.read());
          delay(1);
        }
        Serial.print(msg);
        if(msg.length() > 1) break;
      }

      //Provides the correct UTC offset for the current time
      Serial.println("Sending:AT+TZONE="+String(timezoneOffset*3600));
      Serial1.println("AT+TZONE="+String(timezoneOffset*3600));

      //Wait for "OK" response
      while(1)
      {
        String msg = "";
        while(Serial1.available())
        {
          msg += char(Serial1.read());
          delay(1);
        }
        Serial.print(msg);
        if(msg.length() > 1) break;
      }  
  }
  else
  {
    Serial.println("Connection unsucessful :(\n\n" \
                   "Make sure the WiFi credentials are correct, and the module is in the station mode");
    while(1);
  }
}

void loop() {
  //Get the current time
  Serial.println("Sending:AT+TIME");
  Serial1.println("AT+TIME");

  while(Serial1.available())
  {
    Serial.print(char(Serial1.read()));
    delay(1);
  }

  delay(1000);
}

Set your Board and Serial Port, and then upload the sketch to your Arduino. Then open the serial monitor. Make sure your baud rate is set to 9600. You'll begin to see output.

Getting time output on serial monitor

Troubleshooting

Firmware

If, for any reason, you wish to update the firmware, you can refer to the DA16200 AT Command User Manual for more information on downloading the correct firmware via the AT Command.

Resources and Going Further

Now that you've successfully got your MicroMod ESP Function Board up and running, it's time to incorporate it into your own project! For more information, check out the resources below:

Looking for more inspiration? Check out these other tutorials related to MicroMod.

MicroMod Machine Learning Carrier Board Hookup Guide

Get hacking with this tutorial on our Machine Learning Carrier Board!

MicroMod Asset Tracker Carrier Board Hookup Guide

Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.

MicroMod Ethernet Function Board - W5500 Hookup Guide

Add Ethernet and PoE capabilities to your MicroMod project using the Ethernet Function Board - W5500.

MicroMod Alorium Sno M2 Processor Board Hookup Guide

Get started with the MicroMod Alorium Sno M2 Processor Board!