Wireless Joystick Hookup Guide

≡ Pages
Contributors: Alex the Giant

Hardware Hookup

The first step is to solder in the right angle tactile buttons. These are meant to inserted from the bottom the board and soldered to the top layer of PCB. This will look like the image below.

Bottom view close up of trigger buttons

The way the rest of the board is soldered really depends on what it will be used for. There are few different configurations for the joystick(s) and buttons. Read on to see he different configurations.

Dual Joysticks

In this configuration, the Wireless Joystick uses both joysticks and is perfect for tank steering robots. Tank steering maps the vertical position of the left and right joysticks to the speed and direction of the left and right motors of a robot. After soldering in the joysticks, the board should look like this:

Dual Joysticks

Single Joystick

In this configuration, the Wireless Joystick uses a single joystick on the left and 4 of our 12mm momentary pushbuttons on the right. This setup is similar to what older console game consoles used. After soldering in the joystick and switches, the Wireless Joystick board will look like the image below.

Gamepad configuration

A quick tip about soldering the joystick(s): Sometimes during shipping, the pins on the joystick can be bend slightly. Before trying to insert the pins to the board, make sure all of the pins look straight and run parallel with the others. When soldering the joysticks, start with the pins on the vertical and horizontal potentiometers, and use a pair of tweezers to motivate the pins into place and work my way to the select button.

Mounting the LiPo Battery

To secure the battery to the board, we recommend using a small piece of foam double sided tape. We've found the easiest place to put the battery is under the right joystick. Before mounting the battery, make sure to trim the the joystick solder joints to avoid puncturing the battery!

trimmed solder joints

Trimmed Solder Joints For LiPo Battery

Battery taped

LiPo Battery with Double Sided Foam Tape

Battery mounted

Attached LiPo Battery

Setting the Battery Charge Rate

By default, the charge rate is set to the maximum rate of 500mA. If you're battery is larger than 500mAh, you can skip ahead to the Arduino Examples section. If you're using less than a 500mAh battery, you should solder in the appropriate resistor that we'll determine below.

The life of a lithium battery is dependent on a few factors: number of charge/discharge cycles, charge/discharge rate, battery temperature, as well as a few others. When charging a lithium battery, it's recommended not to exceed a 1C charge rate. For example, if you have a 400mAh battery, your current to charge the battery should not exceed 400mA. To change the rate, move the solder jumper so that the middle and R_PROG pads are shorted. Then solder in the appropriate resistor. To calculate the right resistor, use the equation below:

R_PROG = 1000 / I_PROG

R_PROG = Resistor value in kohms

I_PROG = Desired current value in mA

To charge the battery, simply plug in the micro USB cable, and move the switch to the OFF position. If your charge rate is below 200mA, the board should charge without issue regardless of the power switch position. Faster charge rates may require the switch to be off to cut current to everything but the charging circuit if charging from a computer's USB port or small USB chargers.