Twinkle Zodiac Constellation

≡ Pages
Contributors: Feldi

Introduction

In this project, we’ll create a decorative embroidery hoop using conductive thread to connect LilyPad LEDs to a LilyTiny, powered by a LilyPad battery holder. Follow along by drawing your own design on a piece of fabric, or download and print one of SparkFun’s designs.

Design and build time: 1-2 Hours

Twinkle Zodiac Constellation

Suggested Reading

If this is your first sewable electronics project, we recommend you read our LilyPad Basics tutorial.

LilyPad Basics: E-Sewing

December 17, 2016
Learn how to use conductive thread with LilyPad components.

Materials and Tools

Let's go over all of the things you'll need to sew your project together.

Items required for the Twinkle Zodiac Constellation:

The wishlist is based on one Zodiac pattern. If you plan on making more patterns or are using a pattern that does not require a lot of LEDs, feel free to adjust the quantity as necessary.

You Will Also Need:

  • Embroidery Hoop (size should matches the diameter of your pattern)
  • Lightweight Navy Cotton Fabric
  • Needle
  • Scissors
  • Shearing Scissors
  • Silver Embroidery Floss
  • White Chalk or Colored Pencil
  • Printer and Paper
  • Hot Glue

Planning Your Project

For this project, we have designed a pattern for each zodiac sign for your use! You may notice that the patterns are not all the same size. We learned that some constellations work well on a smaller hoop, while other simply have too many components to fit in the space. Each pattern is at its smallest recommended size. You can scale up from there by editing the files on your own computer. The pattern files are available for download below.

PLANNING

STEP 1

Download and print the provided embroidery pattern for the constellation(s) of your choice, and cut it out along the line with your regular scissors.

Step 1



STEP 2

Use your shearing scissors to cut a swatch of fabric large enough to cover your hoop plus an inch or two. Then stretch it and place it between the hoops.

Step 2



STEP 3

To trace your pattern, place it behind your stretched fabric.

Step 3

Then bring it to a window or light, and mark all of the circles in your design.

Step 4

Now you are ready to start adding LilyPad Components!

Understanding Your Circuit

Before we put our parts to fabric, let's take a look at the LEDs and battery holder. Notice that the silver sew tabs are labeled either positive or negative. Many electronic components like these have polarity, meaning electric current can only flow through them in one direction.

LED Polarity

If hooked up incorrectly, they will not light up. Batteries are also polarized; they have a positive and negative side. Always check the labels on LilyPad pieces to make sure they are correctly oriented before sewing together a circuit.

LED Constellation

The following diagram illustrates the circuit you will be following for your constellation hoop. Notice how the LEDs have been grouped into 3 sets. No matter how many LEDs are included in your design, you will want to divide them into three groups as shown. The '-' tab of every single LED in your constellation connects to the rest with conductive thread, as well as the '-' tab on the LilyPad Tiny and the '-' tab on the battery holder.

The '+' tabs will be treated differently. For each group of LEDs, you will connect all the '+' tabs inside that group with conductive thread, and then connect them to either pins 0, 1, or 3. We are not using pin 2 as the animation is not ideal for this design. This configuration is an example of LEDs in a parallel circuit. For power, you will also need to connect the '+' tab of the battery to the '+' tab of the LilyTiny.

Also, notice that the battery holder and LilyTiny are dulled out in our circuit diagram. That is because they will lie on the backside of your fabric with the LEDs on the top side.

Zodia LilyPad

Arranging Your Circuit

Each circle you marked when tracing the pattern represents where a single LilyPad LED should go. These LEDs should be facing up as seen in the image below.

Glue Hardware

The LilyTiny and LilyPad Battery holder should both be positioned on the opposite side (or back side) as the LEDs. Make sure the components are facing away from the fabric. Please refer to the circuit diagram above for a detailed illustration.

Pins 0, 1, and 3, are connected to 3 LEDs in parallel. You can increase or decrease the number of LEDs in parallel attached to any given pin depending on your constellations pattern and component count. The maximum LEDs I have connected to a single pin for this project is 6.

Plot your LEDs, LilyTiny, and battery holder in an arrangement on the fabric that allows you to sew the parts together according to the circuit diagram provided above, and glue them down with hot glue.

Note: Notice that pin 2 is not being used. This pin has a built in breathing or heart beat animation when connected to an LED. While a lovely animation - it doesn't suit the purpose of this project, so we are sticking to pins 0,1, and 3.
Remember: Glue is great for keeping your components in place, but it can interfere with your circuit. Try to keep glue clear of sew tabs.

Stitching It Together

If you need help sewing with conductive thread, this tutorial covers the basics.

STEP 1:

Cut a long piece of conductive thread and thread the needle with it. Tie a knot at the end. Begin to connect sewable tabs with the thread according to the circuit diagram provided above.

sew circuit

STEP 2:

When you are finished, making sure your fabric is taut. To test the circuit, pop a battery inside your holder and turn it on to troubleshoot. If any of your LEDs are not working, this is the time to figure out why and fix it based on information provided from the tutorial in the suggested reading.

If you are satisfied and your circuit works well, use hot glue or clear nail polish to seal knots and frayed thread to avoid shorts. For more information about insulation techniques for e-textiles, check out this tutorial.

test and seal

STEP 3:

Use the shearing scissors to cut out a second piece of fabric, the same size as the first. With your hoop laying on a flat, clean surface, gently unscrew the the fastener at the top of the embroidery hoop and remove the outer circle. Place your second sheet of fabric directly on top of the piece of fabric with your LEDs, and stretch them together in the hoop.

add second sheet

STEP 4:

Turn the battery switch to the 'ON' position so that you can see the LEDs through the top piece of fabric. Using a straight edge and white pencil, begin to draw lines connecting each LED according the pattern.

draw lines

STEP 5:

Cut a piece of silver embroidery floss and thread the needle with it. Turn the battery switch off and begin to sew the silver embroidery floss over the drawn lines using a backstitch. During this step, you will essentially sew the two pieces of fabric together. Make sure by this point that the circuit is working without any issues because you will not be able to make adjustments or access the LEDs after.

sew lines

STEP 6:

Take your pattern and cut the bottom quarter (with the text) off. Then, loosen your hoop again and fold back the bottom most piece of fabric (the one with the electronics attached) where the text should go. Tighten the hoop back up with the fabric bent back like the picture below, and place the bottom part of you pattern behind the top sheet.

prepare for letters

STEP 7:

Bring this to a window or other light source and trace the letters from the pattern. Then replace the folded piece of fabric back to the original position. Make sure to stretch the fabric again every time you loosen and tighten your hoop.

trace letters

STEP 8:

Stitch over the letter traces using the silver embroidery floss.

sew letters

STEP 9:

Make sure your fabric is nice and taut with your hoop. Once the fabric is tight in the hoop, cut away the excess fabric around the hoop.

Trim Fabric

STEP 10:

Turn the power on, hang up, and enjoy!

completed project

Resources and Going Further

These tutorials will guide you through concepts and advanced projects:

Insulation Techniques for e-Textiles

Learn a few different ways to protect your conductive thread and LilyPad components in your next wearables project.

Planning a Wearable Electronics Project

Tips and tricks for brainstorming and creating a wearables project.

Choosing a LilyPad Arduino for Your Project

Not sure which LilyPad Arduino is right for you? We'll discuss the features of each and help you decide.

LilyPad Basics: E-Sewing

Learn how to use conductive thread with LilyPad components.

Marquee Party Bag

This tutorial provides everything you need to know to make your own Marquee Party Bag!

Fairy LED Bracelet

Light up the world - and your wrist - with this quick and easy rechargeable firefly LED bracelet.

LED PomPom Headbands

Follow this tutorial to make your own light up PomPom headband! Try the beginner version if you are new to electronics or the advanced version if you have some more experience!