TSH82 Configurable OpAmp Hookup Guide

≡ Pages
Contributors: Pete-O

Introduction

The TSH82 Configurable OpAmp board was designed to give you the best combination of performance and flexibility that we could achieve. The TSH82 device itself has 2 gain stages, each one independently accessible via header. Each stage is natively configured as an inverting amplifier, giving you a gain of -4.7 with AC input coupling. Stringing both stages together gives you a gain of about 22. But with the use of the jumpers on the back of the board, you can additionally configure each stage for non-inverting operation, differential input, and DC input coupling. The board will also operate with a single-ended DC power supply of 4.5V to 12V, or a bipolar supply from +/-2.25V to +/-6V.

SparkFun Configurable OpAmp Board - TSH82

BOB-14874
$7.95

Required Materials

In order to get signals in and out of the board, you're going to have to solder some stuff together. You may not need everything on this list, depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Suggested materials

In order to tailor the board to your specifications, you might want some other parts that we can offer.

Resistor Kit - 1/4W (500 total)

COM-10969
$9.95

Straight Header - Female (PTH, 0.1in., 40-Pin)

PRT-00115
$1.95

Right Angle Header - Male (PTH, 0.1in., 40-Pin)

PRT-00553
$2.50

Electrolytic Decoupling Capacitors - 10uF/25V

COM-00523
$0.55

Rotary Potentiometer - 100k Ohm, Linear (Panel Mount)

COM-14622
$3.50

Rotary Potentiometer - 250k Ohm, Logarithmic (Panel Mount)

COM-14623
Retired

You may also want to examine these signals in real time as you're working with them, or maybe generate a signal to run through your opamp board.

Frequency Generator Kit - FG085

KIT-11394
Retired

SparkFun MiniGen - Pro Mini Signal Generator Shield

BOB-11420
Retired

Digilent Analog Discovery 2

TOL-13929
Retired
Digital Storage Oscilloscope - 100MHz (TBS2104)

Digital Storage Oscilloscope - 100MHz (TBS2104)

TOL-14925
Retired

Suggested Reading

If any of this is new to you, have a look through these - the OpAmp intro with LT Spice is particularly good as an opamp primer.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Working with Wire

How to strip, crimp, and work with wire.

How to Use an Oscilloscope

How to work the dials and buttons on an oscilloscope, and a glossary of the o-scope lexicon.

Introduction to Operational Amplifiers with LTSpice

Picking up where we left off in "Getting Started with LTSpice," we delve a little deeper into LTSpice through an introduction of Operational Amplifiers (OpAmps).