Tinker Kit Circuit Guide

≡ Pages
Contributors: Joel_E_B, bboyho, El Duderino

Circuit 4: RGB Night-Light

In this circuit, you'll take the night-light concept to the next level by adding an RGB LED, which is three differently colored Light-Emitting Diodes (LEDs) built into one component. RGB stands for Red, Green and Blue, and these three colors can be combined to create any color of the rainbow!

Tinker Kit Circuit 4

Parts Needed

You will need the following parts:

  • 1x Breadboard
  • 1x SparkFun RedBoard
  • 12x Jumper Wires
  • 1x LED - RGB Diffused Common Cathode
  • 3x 330Ω Resistor
  • 1x 10K Potentiometer
  • 1x Photoresistor
  • 1x 10kΩ Resistor

Didn't Get the Tinker Kit?

If you are conducting this experiment and didn't get the Tinker Kit, we suggest using these parts:

Trimpot 10K Ohm with Knob

COM-09806
$1.25

SparkFun RedBoard Qwiic

DEV-15123
$21.95

Breadboard - Self-Adhesive (White)

PRT-12002
$6.25

LED - RGB Diffused Common Cathode

COM-09264
$2.30

Jumper Wires Standard 7" M/M - 30 AWG (30 Pack)

PRT-11026
$3.50

Mini Photocell

SEN-09088
$1.75

Resistor 10K Ohm 1/4 Watt PTH - 20 pack (Thick Leads)

PRT-14491
$1.50

Resistor 330 Ohm 1/4 Watt PTH - 20 pack (Thick Leads)

PRT-14490
$1.25

New Components

RGB LED

An RGB LED is actually three small LEDs --- one red, one green and one blue --- inside a normal LED housing. The RGB LED included in this kit has all the internal LEDs share the same ground wire, so there are four legs in total. To turn one color on, ensure ground is connected, then power one of the legs just as you would a regular LED. If you turn on more than one color at a time, you will see the colors start to blend together to form a new color.

RGB LED

New Concepts

Analog Output (Pulse-width Modulation)

You can use the digitalWrite() command to turn pins on the RedBoard on (5V) or off (0V), but what if you want to output 2.5V? The RedBoard doesn't have an Analog Output, but it is really good at switching some digital pins on and off fast enough to simulate an analog output. analogWrite() can output 2.5 volts by quickly switching a pin on and off so that the pin is only on 50 percent of the time (50% of 5V is 2.5V). By changing the percent of time that a pin is on, from 0 percent (always off) to 100 percent (always on), analogWrite() can output any voltage between 0 and 5V. This is known as pulse-width modulation (or PWM). By using PWM, you can create many different colors with the RGB LED.

Digital (PWM~): Only a few of the pins on the RedBoard have the circuitry needed to turn on and off fast enough for PWM. These are pins 3, 5, 6, 9, 10 and 11. Each PWM pin is marked with a ~ on the board. Remember, analogWrite() can only used on these pins.

Creating Your Own Simple Functions

When programmers want to use a piece of code over and over again, they write a function. The simplest functions are just chunks of code that you give a name to. When you want to run that code, you can “call” the function by typing its name, instead of writing out all of the code. More complicated functions take and return pieces of information from the program (we call these pieces of information parameters). In this circuit, you'll write functions to turn the RGB LED different colors by just typing that color's name.

Hardware Hookup

Polarized Components Pay special attention to the component’s markings indicating how to place it on the breadboard. Polarized components can only be connected to a circuit in one direction.

Just like a regular LED, an RGB LED is polarized and only allows electricity to flow in one direction. Pay close attention to the flat edge and to the different length leads. Both are indicators to help orient the LED correctly.

RGB LED Pins

Ready to start hooking everything up? Check out the circuit diagram and hookup table below to see how everything is connected.

Circuit Diagram

Circuit 4 Fritzing diagram

Having a hard time seeing the circuit? Click on the image for a closer look.

Hookup Table

Component RedBoard Breadboard Breadboard Breadboard Breadboard
RGB LED A5 (RED) A4 (GND) A3 (GREEN) A2 (BLUE)
330Ω Resistor
(orange, orange, brown)
E2 F2
330Ω Resistor
(orange, orange, brown)
E3 F3
330Ω Resistor
(orange, orange, brown)
E5 F5
Jumper Wire E4 GND Rail ( - )
Jumper Wire Digital Pin 9 J5
Jumper Wire Digital Pin 10 J3
Jumper Wire Digital Pin 11 J2
Jumper Wire 5V 5V Rail ( + )
Jumper Wire GND GND Rail ( - )
Potentiometer B15 B16 B17
Jumper Wire Analog Pin 1 (A1) E16
Jumper Wire E15 5V Rail ( + )
Jumper Wire E17 GND Rail ( - )
Photoresistor A26 B25
10kΩ Resistor
(brown, black, orange)
C26 D27
Jumper Wire Analog Pin 0 (A0) E26
Jumper Wire E25 5V Rail ( + )
Jumper Wire E27 GND Rail ( - )

In the table, polarized components are shown with a warning triangle and the whole row highlighted yellow.

Open the Sketch

Open the example code from your Arduino sketchbook or copy and paste the following code into the Arduino IDE. Hit upload, and see what happens!

language:cpp
/*
SparkFun Tinker Kit
Circuit 4: RGB Night-Light

Turns an RGB LED on or off based on the light level read by a photoresistor.
Change colors by turning the potentiometer.

This sketch was written by SparkFun Electronics, with lots of help from the Arduino community.
This code is completely free for any use.

View circuit diagram and instructions at: https://learn.sparkfun.com/tutorials/activity-guide-for-sparkfun-tinker-kit/
Download drawings and code at: https://github.com/sparkfun/SparkFun_Tinker_Kit_Code
 */

int photoresistor;          //variable for storing the photoresistor value
int potentiometer;          //variable for storing the photoresistor value
int threshold = 700;            //if the photoresistor reading is lower than this value the light wil turn on

//LEDs are connected to these pins
int RedPin = 9;
int GreenPin = 10;
int BluePin = 11;

void setup() {
  Serial.begin(9600);           //start a serial connection with the computer

  //set the LED pins to output
  pinMode(RedPin,OUTPUT);
  pinMode(GreenPin,OUTPUT);
  pinMode(BluePin,OUTPUT);
}

void loop() {

  photoresistor = analogRead(A0);         //read the value of the photoresistor
  potentiometer = analogRead(A1);

  Serial.print("Photoresistor value:");
  Serial.print(photoresistor);          //print the photoresistor value to the serial monitor
  Serial.print("  Potentiometer value:");
  Serial.println(potentiometer);          //print the photoresistor value to the serial monitor

  if(photoresistor < threshold){          //if it's dark (the photoresistor value is below the threshold) turn the LED on
    //These nested if staments check for a variety of ranges and 
    //call different functions based on the current potentiometer value.
    //Those functions are found at the bottom of the sketch. 
    if(potentiometer > 0 && potentiometer <= 150)
      red();
    if(potentiometer > 150 && potentiometer <= 300)
      orange();
    if(potentiometer > 300 && potentiometer <= 450)
      yellow(); 
    if(potentiometer > 450 && potentiometer <= 600)
      green();
    if(potentiometer > 600 && potentiometer <= 750)
      cyan();
    if(potentiometer > 750 && potentiometer <= 900)
      blue(); 
    if(potentiometer > 900)
      magenta();  
  } 
  else {                                //if it isn't dark turn the LED off

    turnOff();                            //call the turn off function

  }  

  delay(100);                             //short delay so that the printout is easier to read
}

void red (){

    //set the LED pins to values that make red    
    analogWrite(RedPin, 100);
    analogWrite(GreenPin, 0);
    analogWrite(BluePin, 0);
}
void orange (){

    //set the LED pins to values that make orange
    analogWrite(RedPin, 100);
    analogWrite(GreenPin, 50);
    analogWrite(BluePin, 0);
}
void yellow (){

    //set the LED pins to values that make yellow
    analogWrite(RedPin, 100);
    analogWrite(GreenPin, 100);
    analogWrite(BluePin, 0);
}
void green (){

    //set the LED pins to values that make green    
    analogWrite(RedPin, 0);
    analogWrite(GreenPin, 100);
    analogWrite(BluePin, 0);
}
void cyan (){

    //set the LED pins to values that make cyan    
    analogWrite(RedPin, 0);
    analogWrite(GreenPin, 100);
    analogWrite(BluePin, 100);
}
void blue (){

    //set the LED pins to values that make blue
    analogWrite(RedPin, 0);
    analogWrite(GreenPin, 0);
    analogWrite(BluePin, 100);
}
void magenta (){

    //set the LED pins to values that make magenta   
    analogWrite(RedPin, 100);
    analogWrite(GreenPin, 0);
    analogWrite(BluePin, 100);
}
void turnOff (){

    //set all three LED pins to 0 or OFF
    analogWrite(RedPin, 0);
    analogWrite(GreenPin, 0);
    analogWrite(BluePin, 0);
}

What You Should See

This sketch is not dissimilar from the last. It reads the value from the photoresistor, compares it to a threshold value, and turns the RGB LED on or off accordingly. This time, however, we've added a potentiometer back into the circuit. When you twist the pot, you should see the color of the RGB LED change based on the pot's value.

Circuit 4 demo photo

Open the Serial Monitor. The value being read by the light sensor should be printed several times a second. When you turn out the lights or cover the sensor, the LED will shine whatever color your programmed in your color function. Next to the light value, you'll see the potentiometer value print out as well.

Note: If the room you are in is very bright or dark, you may have to change the value of the “threshold” variable in the code to make your night-light turn on and off. See the Troubleshooting section for instructions.

Program Overview

  1. Store the light level from pin A0 in the variable photoresistor.
  2. Store the potentiometer value from pin A1 in the variable potentiometer.
  3. If the light level variable is above the threshold, call the function that turns the RGB LED off.
  4. If the light level variable is below the threshold, call one of the color functions to turn the RGB LED on.
  5. If potentiometer is between 0 and 150, turn the RGB LED on red.
  6. If potentiometer is between 151 and 300, turn the RGB LED on orange.
  7. If potentiometer is between 301 and 450, turn the RGB LED on yellow.
  8. If potentiometer is between 451 and 600, turn the RGB LED on green.
  9. If potentiometer is between 601 and 750, turn the RGB LED on cyan.
  10. If potentiometer is between 751 and 900, turn the RGB LED on blue.
  11. If potentiometer is greater than 900, turn the RGB LED on magenta.

Code to Note

CodeDescription
Analog Output (PWM):
analogWrite(RedPin, 100);
The analogWrite() function outputs a voltage between 0 and 5V on a pin. The function breaks the range between 0 and 5V into 255 little steps. Note that we are not turning the LED on to full brightness (255) in this code so that the night-light is not too bright. Feel free to change these values and see what happens.
Nested if Statements:
if(logic statement) {
if(logic statement) {
code to be run if the logic statement is true}
if(logic statement) {
code to be run if the logic statement is true}
}
A nested if statement is one or more if statements "nested" inside of another if statement. If the parent if statement is true, then the code looks at each of the nested if statements and executes any that are true. If the parent if statement is false, then none of the nested statements will execute.
More Logical Operators:
if(potentiometer > 0 && potentiometer <= 150)
These if statements are checking for two conditions by using the AND (&&) operator. In this line, the if statement will only be true if the value of the variable potentiometer is greater than 0 AND if the value is less than or equal to 150. By using &&, the program allows the LED to have many color states.
Defining a Function:
void function_name () {
code to run inside function }
This simple version of a function executes the code inside the curly brackets whenever the name is written in the main program.
Calling a Function:
function_name();
Calls a function that you have created. In a later circuit, you will learn how to make more complicated functions that take data from the main program (these pieces of data are called parameters).

Coding Challenges

ChallengeDescription
Add more colorsYou can create many more colors with the RGB LED. Use the analogWrite() function to blend different values of red, green and blue together to make even more colors. You can divide the potentiometer value up more and make more nested if statements so that you can have more colors as you twist the knob.
Multi color blinkTry using delays and multiple color functions to have your RGB LED change between multiple colors.
Change the thresholdTry setting your threshold variable by reading the value of a potentiometer with analogRead(). By turning the potentiometer, you can then change the threshold level and adjust your night-light for different rooms.
Fading the LEDTry using a loop with the analogWrite() to get your LED to pulse gently or smoothly transition between colors.

Troubleshooting

ProblemSolution
The LED never turns on or offOpen the Serial Monitor in Arduino and make sure that your photoresistor is returning values between 0 and 1023. Try covering the photoresistor; the values should change. If they do not change, check the wiring of the photoresistor.
If your photoresistor is working correctly, make sure that your threshold variable sits in between the value that the photoresistor reads when it is bright and the value that the photoresistor reads when it is dark (e.g., bright = 850, dark = 600, threshold = 700).
My LED doesn’t show the colors that I expectMake sure that all three of the pins driving your RGB LED are set to OUTPUT, using the pinMode() command in the setup section of the code. Then make sure that each LED is wired properly.
Nothing is printing in the Serial MonitorTry unplugging your USB cable and plugging it back in. In the Arduino IDE, go to Tools > Port, and make sure that you select the right port.