SparkFun Triple Axis Accelerometer Breakout - BMA400 (Qwiic) Hookup Guide
Contributors:
El Duderino
Resources and Going Further
That's all for this tutorial. For more information about the BMA400 and these breakouts, check out the resources below:
- Schematics
- Eagle Files
- Board Dimensions
- Datasheet (BMA400)
- Qwiic Info Page
- BMA400 Arduino Library
- GitHub Hardware Repo
Need some inspiration for your a motion-sensing project using the BMA400? The tutorials below may help you come up with some ideas:
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.
TFMini - Micro LiDAR Module Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders.
Advanced Autonomous Kit for Sphero RVR Assembly Guide
Get your Advanced Autonomous Kit for the Sphero RVR built up with this hookup guide!
Qwiic 6DoF (LSM6DSO) Breakout Hookup Guide
A hookup guide for the Qwiic 6DoF (LSM6DSO), which features a 3-axis accelerometer, 3-axis gyroscope, temperature sensor, and FIFO buffer.