SparkFun Qwiic GPIO Hookup Guide

≡ Pages
Contributors: El Duderino, Englandsaurus

Python Examples

With the Qwiic GPIO Python Package installed, we can start working with the examples included with it. In this section we'll go over each example and highlight pertinent bits of code. To run the examples, download or copy the code into a file then open/save the example file (if needed) and execute the code in your preffered Python IDE.

Qwiic GPIO Example 1

This example sets up all eight I/O pins as outputs and toggles them on and off each second. Note you need to define the mode of each pin as well as call setMode to write the configuration to the Qwiic GPIO. Copy the code below and execute it in your chosen Python IDE.

language:python
from __future__ import print_function
import qwiic_gpio
import time
import sys

def runExample():

    print("\nSparkFun Qwiic GPIO Example 1\n")
    myGPIO = qwiic_gpio.QwiicGPIO()

    if myGPIO.isConnected() == False:
        print("The Qwiic GPIO isn't connected to the system. Please check your connection", \
            file=sys.stderr)
        return

    myGPIO.begin()
    myGPIO.mode_0 = myGPIO.GPIO_OUT
    myGPIO.mode_1 = myGPIO.GPIO_OUT
    myGPIO.mode_2 = myGPIO.GPIO_OUT
    myGPIO.mode_3 = myGPIO.GPIO_OUT
    myGPIO.mode_4 = myGPIO.GPIO_OUT
    myGPIO.mode_5 = myGPIO.GPIO_OUT
    myGPIO.mode_6 = myGPIO.GPIO_OUT
    myGPIO.mode_7 = myGPIO.GPIO_OUT
    myGPIO.setMode()

    while True:
        myGPIO.out_status_0 = myGPIO.GPIO_HI
        myGPIO.out_status_1 = myGPIO.GPIO_HI
        myGPIO.out_status_2 = myGPIO.GPIO_HI
        myGPIO.out_status_3 = myGPIO.GPIO_HI
        myGPIO.out_status_4 = myGPIO.GPIO_HI
        myGPIO.out_status_5 = myGPIO.GPIO_HI
        myGPIO.out_status_6 = myGPIO.GPIO_HI
        myGPIO.out_status_7 = myGPIO.GPIO_HI
        myGPIO.setGPIO()
        print("set hi")
        time.sleep(1)
        myGPIO.out_status_0 = myGPIO.GPIO_LO
        myGPIO.out_status_1 = myGPIO.GPIO_LO
        myGPIO.out_status_2 = myGPIO.GPIO_LO
        myGPIO.out_status_3 = myGPIO.GPIO_LO
        myGPIO.out_status_4 = myGPIO.GPIO_LO
        myGPIO.out_status_5 = myGPIO.GPIO_LO
        myGPIO.out_status_6 = myGPIO.GPIO_LO
        myGPIO.out_status_7 = myGPIO.GPIO_LO
        myGPIO.setGPIO()
        print("set lo")
        time.sleep(1)


if __name__ == '__main__':
    try:
        runExample()
    except (KeyboardInterrupt, SystemExit) as exErr:
        print("\nEnding Example 1")
        sys.exit(0)

Qwiic GPIO Example 2

Example 2 shows how to read each I/O pin when they are configured as inputs. It first sets up all pins using the setMode function as we did in Example 1. The code then monitors and prints out the status of each input every 0.25 seconds. You can copy the entire example below or open it from your downloaded copy of the Python package:

language:python
from __future__ import print_function
import qwiic_gpio
import time
import sys


def runExample():

    print("\nSparkFun Qwiic GPIO Example 2\n")
    myGPIO = qwiic_gpio.QwiicGPIO()

    if myGPIO.isConnected() == False:
        print("The Qwiic GPIO isn't connected to the system. Please check your connection",
              file=sys.stderr)
        return

    myGPIO.begin()
    myGPIO.mode_0 = myGPIO.GPIO_IN
    myGPIO.mode_1 = myGPIO.GPIO_IN
    myGPIO.mode_2 = myGPIO.GPIO_IN
    myGPIO.mode_3 = myGPIO.GPIO_IN
    myGPIO.mode_4 = myGPIO.GPIO_IN
    myGPIO.mode_5 = myGPIO.GPIO_IN
    myGPIO.mode_6 = myGPIO.GPIO_IN
    myGPIO.mode_7 = myGPIO.GPIO_IN
    myGPIO.setMode()

    while True:
        myGPIO.getGPIO() #This function updates each in_status_x variable
        print("GPIO 0:", end=" ")
        print(myGPIO.in_status_0, end=" ")
        print("GPIO 1:", end=" ")
        print(myGPIO.in_status_1, end=" ")
        print("GPIO 2:", end=" ")
        print(myGPIO.in_status_2, end=" ")
        print("GPIO 3:", end=" ")
        print(myGPIO.in_status_3, end=" ")
        print("GPIO 4:", end=" ")
        print(myGPIO.in_status_4, end=" ")
        print("GPIO 5:", end=" ")
        print(myGPIO.in_status_5, end=" ")
        print("GPIO 6:", end=" ")
        print(myGPIO.in_status_6, end=" ")
        print("GPIO 7:", end=" ")
        print(myGPIO.in_status_7)
        time.sleep(.25)

if __name__ == '__main__':
    try:
        runExample()
    except (KeyboardInterrupt, SystemExit) as exErr:
        print("\nEnding Example 1")
        sys.exit(0)

Qwiic GPIO Example 3

Example 3 demonstrates how to invert an I/O pin configured as an input. We first set all eight pins as inputs and then invert half of them using the setInversion(self) function. As we covered in the Arduino Examples section, each I/O pin set as an input defaults to an active HIGH input so inverting it switches it to an active LOW input. Again, note that you need to define the inversion status of each pin you wish to invert and then write that data using the setInversion function.

language:python
from __future__ import print_function
import qwiic_gpio
import time
import sys


def runExample():

    print("\nSparkFun Qwiic GPIO Example 3\n")
    myGPIO = qwiic_gpio.QwiicGPIO()

    if myGPIO.isConnected() == False:
        print("The Qwiic GPIO isn't connected to the system. Please check your connection",
              file=sys.stderr)
        return

    myGPIO.begin()
    myGPIO.mode_0 = myGPIO.GPIO_IN
    myGPIO.mode_1 = myGPIO.GPIO_IN
    myGPIO.mode_2 = myGPIO.GPIO_IN
    myGPIO.mode_3 = myGPIO.GPIO_IN
    myGPIO.mode_4 = myGPIO.GPIO_IN
    myGPIO.mode_5 = myGPIO.GPIO_IN
    myGPIO.mode_6 = myGPIO.GPIO_IN
    myGPIO.mode_7 = myGPIO.GPIO_IN
    myGPIO.setMode()

    myGPIO.inversion_0 = myGPIO.INVERT
    myGPIO.inversion_1 = myGPIO.NO_INVERT
    myGPIO.inversion_2 = myGPIO.INVERT
    myGPIO.inversion_3 = myGPIO.NO_INVERT
    myGPIO.inversion_4 = myGPIO.INVERT
    myGPIO.inversion_5 = myGPIO.NO_INVERT
    myGPIO.inversion_6 = myGPIO.INVERT
    myGPIO.inversion_7 = myGPIO.NO_INVERT
    myGPIO.setInversion()

    while True:
        myGPIO.getGPIO()  # This function updates each in_status_x variable
        print("GPIO 0:", end=" ")
        print(myGPIO.in_status_0, end=" ")
        print("GPIO 1:", end=" ")
        print(myGPIO.in_status_1, end=" ")
        print("GPIO 2:", end=" ")
        print(myGPIO.in_status_2, end=" ")
        print("GPIO 3:", end=" ")
        print(myGPIO.in_status_3, end=" ")
        print("GPIO 4:", end=" ")
        print(myGPIO.in_status_4, end=" ")
        print("GPIO 5:", end=" ")
        print(myGPIO.in_status_5, end=" ")
        print("GPIO 6:", end=" ")
        print(myGPIO.in_status_6, end=" ")
        print("GPIO 7:", end=" ")
        print(myGPIO.in_status_7)
        time.sleep(.25)

if __name__ == '__main__':
    try:
        runExample()
    except (KeyboardInterrupt, SystemExit) as exErr:
        print("\nEnding Example 1")
        sys.exit(0)