SparkFun MicroMod Input and Display Carrier Board Hookup Guide

≡ Pages
Contributors: Alex the Giant, Ell C

Software Setup and Programming

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

To get started, you're going to want to get familiar with our HyperDisplay libraries. HyperDisplay is an abstracted library for pretty much any 2D graphics display and has a focus on extensibility. Since the interface is standardized you can write display applications just once and make them work on many different displays with a few small changes. If you want to go more in depth check out this HyperDisplay tutorial.

Everything You Should Know About HyperDisplay

February 20, 2019
This is a tutorial to go in-depth about the SparkFun HyperDisplay Arduino Library.

To use HyperDisplay with this carrier board, you will need to have all three of the following libraries installed in your Arduino IDE. You can head on over to the individual GitHub pages to download or simply click the appropriate link for each of the libraries listed below:

Library Name Arduino Library Manager Search Term GitHub Link Download Link
HyperDisplay SparkFun HyperDisplay HyperDisplay GitHub HyperDisplay Download
HyperDisplay ILI9341 SparkFun HyperDisplay ILI9341 Arduino Library SparkFun HyperDisplay ILI9341 Arduino Library GitHub SparkFun HyperDisplay ILI9341 Arduino Library Download
HyperDisplay 4DLCD-320240 Arduino Library SparkFun_HyperDisplay_4DLCD-320240_ArduinoLibrary HyperDisplay 4DLCD-320240 Arduino Library GitHub HyperDisplay 4DLCD-320240 Arduino Library Download

Check out this tutorial on how to install an Arduino library if you are unfamiliar.

Each of the libraries above contain some examples, however the ones that will actually make your Input and Display Carrier Board light up are contained in the 'HyperDisplay 4DLCD-320240 Arduino Library' -- in case you are wondering, that name comes from the name of the display module that is used on the board. Once your libraries have been installed move on to the next section and try out a few of the examples.