SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide

≡ Pages
Contributors: Ell C

Hardware Overview

ENS160 Digital Metal-Oxide Multi-Gas Sensor

The ENS160 from ScioSense is a digital multi-gas sensor consisting of four independent heaters and gas sensor elements based on metal oxide (MOX) technology, and a controller. TrueVOC® air quality detection provides outputs such as eCO2, TVOC and AQI in compliance with worldwide IAQ standards.

The ENS160 includes a standard 2-wire digital I2C interface (SCL, SDA) or 4-wire digital SPI interface (SCLK, MOSI, MISO, CSn) for communication to the main host processor. For more information, refer to the datasheet.

The ENS160 Sensor is in the middle of the front of the board

Qwiic Connectors

Our Qwiic Ecosystem makes sensors pretty much plug and play. There are two Qwiic connectors on either side of the Indoor Air Quality Sensor - ENS160 Sensor board to provide power and I2C connectivity simultaneously.

Qwiic connectors are on either side of the board

Power

Ideally, power will be supplied via the Qwiic connectors on either side of the board. Alternatively, power can be supplied through the header along the bottom side of the board labeled 3V3 and GND. The ENS160 functions at 1.8V so an on-board regulator

VDD input range is 1.71-1.98V, VDDIO input range is 1.71-3.6V.

Power pins are the bottom two left pins

I2C Pins

The I2C pins break out the functionality of the Qwiic connectors. Depending on your application, you can connect to these pins via the plated through holes for SDA and SCL.

SDA and SCL are the two pins just to the right of the power pins

ADDR/POCI, Chip Select, and Interrupt Pins

The ADDR/POCI and Chip Select Pins are for use with SPI functionality. The interrupt pin is broken out to use for triggered events.

In this order from the right side of the board

Power LED

When power is supplied to the board, this LED will light up.

Power LED is near the top of the right side of the board

Jumpers

I2C Jumper

Like our other Qwiic boards, the Indoor Air Quality Sensor comes equipped with pull-up resistors on the clock and data pins. If you are daisy-chaining multiple Qwiic devices, you will want to cut this jumper; if multiple sensors are connected to the bus with the pull-up resistors enabled, the parallel equivalent resistance will create too strong of a pull-up for the bus to operate correctly. As a general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected to the bus. To disable the pull up resistors, use an X-acto knife to cut the joint between the two jumper pads highlighted below.

I2C Jumper is the top middle jumper on the back of the board

Address Jumper

By default, the 7-bit un-shifted I2C address of the board is 0x53. However, by manipulating the jumper on the back of the board, this address can be changed:

ADDR
VDD 0x53 (Default)
GND 0x52
OPEN Undefined

Address Jumper is the bottom jumper on the back middle of the board

LED Jumper

If power consumption is an issue, cutting this jumper will disable the Power LED on the front of the board.

LED Jumper is on the far left side of the back of the board

Board Outline

Like most of our standard Qwiic boards, the SparkFun Indoor Air Quality Sensor - ENS160 measures 1 inch by 1 inch.

This board measures 1 inch by 1 inch

Having a hard time seeing the details? Click the image for a closer look.