SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide

≡ Pages
Contributors: Ell C

Example 3: Temp RH Compensation

This example shows how to give the ENS160 Temperature and Relative Humidity Data for compensation. Note that the values that are given for compensation are not populated in their registers until the Air Quality Sensor is set to "Standard" operation and when data is ready i.e. the data ready bit is set. Also note that there will be some rounding of the temperature and relative humidity values when they're given to the sensor and again when they're read back.

Go ahead and open up File->Examples->SparkFun Indoor Air Quality Sensor - ENS160->example3_temp_rh_compensation. Make sure to select your board (SparkFun RedBoard) and COM port before hitting upload to begin experimenting with the air quality sensor.

This image just shows the menu location listed above

Alternatively, you can copy and paste the code below into a nice new Arduino sketch:

language:c
/* example3_temp_rh_compensation.ino

 This example shows how to give the ENS160 Temperature and Relative Humidity
 Data for compensation. Note that the values that are given for compensation are not
 populated in their registers until the Air Quality Sensor is set to "Standard" operation
 and when data is ready i.e. the data ready bit is set. Also note that there will be some 
 rounding of the temperature and relative humidity values when they're given to the sensor
 and again when they're read back. 

 Written by: 
    Elias Santistevan @ SparkFun Electronics October, 2022

 Products: 
  Air Quality Sensor              -  https://www.sparkfun.com/products/20844
  Humidity and Temperature Sensor -  https://www.sparkfun.com/products/16467

 Repository:
    https://github.com/sparkfun/SparkFun_Indoor_Air_Quality_Sensor-ENS160_Arduino_Library

 SparkFun code, firmware, and software is released under the MIT
 License(http://opensource.org/licenses/MIT).

*/
#include <Wire.h>
#include "SparkFun_ENS160.h"
#include "SparkFun_SHTC3.h" // Click here to get the library: http://librarymanager/All#SparkFun_SHTC3

SHTC3 mySHTC3;              // Humidity and Temp Sensor.

SparkFun_ENS160 myENS; 

bool printedCompensation = false; 
int ensStatus; 

float rh;
float tempC; 
SHTC3_Status_TypeDef result; 


void setup()
{
    Wire.begin();

    Serial.begin(115200);

    if( !myENS.begin() )
    {
        Serial.println("Air Quality Sensor did not begin.");
        while(1);
    }

    if( mySHTC3.begin() != SHTC3_Status_Nominal )
    {
        Serial.println("Humidity and Temperature Sensor did not begin.");
        while(1);
    }

    // Reset the indoor air quality sensor's settings.
    if( myENS.setOperatingMode(SFE_ENS160_RESET) )
        Serial.println("Ready.");

    delay(100);

    // Device needs to be set to idle to apply any settings.
    myENS.setOperatingMode(SFE_ENS160_IDLE);

    mySHTC3.update(); // Send command to take a measurement
    if( mySHTC3.lastStatus != SHTC3_Status_Nominal )
    {
        Serial.println("Humidity and Temperature Sensor is not ready.");
        while(1);
    }

    rh = mySHTC3.toPercent();
    tempC = mySHTC3.toDegC();
    Serial.print("Relative Humidity: ");
    Serial.println(rh);
    Serial.print("Temperature(Celsius): ");
    Serial.println(tempC);

    // Give values to Air Quality Sensor. 
    myENS.setTempCompensationCelsius(tempC); 
    myENS.setRHCompensationFloat(rh); 

    delay(500);

    // Set to standard operation
    // Others include SFE_ENS160_DEEP_SLEEP and SFE_ENS160_IDLE
    myENS.setOperatingMode(SFE_ENS160_STANDARD);

    // There are four values here: 
    // 0 - Operating ok: Standard Opepration
    // 1 - Warm-up: occurs for 3 minutes after power-on.
    // 2 - Initial Start-up: Occurs for the first hour of operation.
  //                                                and only once in sensor's lifetime.
    // 3 - No Valid Output
    ensStatus = myENS.getFlags();
    Serial.print("Gas Sensor Status Flag: ");
    Serial.println(ensStatus);

}

void loop()
{
    if( myENS.checkDataStatus() )
    {

        if( printedCompensation == false)
        {
            Serial.println("---------------------------");
            Serial.print("Compensation Temperature: ");
            Serial.println(myENS.getTempCelsius());
            Serial.println("---------------------------");
            Serial.print("Compensation Relative Humidity: ");
            Serial.println(myENS.getRH());
            Serial.println("---------------------------");
            printedCompensation = true;
            delay(500);
        }

        Serial.print("Air Quality Index (1-5) : ");
        Serial.println(myENS.getAQI());

        Serial.print("Total Volatile Organic Compounds: ");
        Serial.print(myENS.getTVOC());
        Serial.println("ppb");

        Serial.print("CO2 concentration: ");
        Serial.print(myENS.getECO2());
        Serial.println("ppm");

    }

    delay(200);
}

Your hardware hookup should look something like the following:

Daisy chained Air Quality Sensor and SHTC3 Humidity Sensor

Once you've got your code uploaded, open up a Serial Monitor and check out your output. You should see something like the following:

Output of example 3