SparkFun GPS-RTK Dead Reckoning ZED-F9K Hookup Guide

≡ Pages
Contributors: bboyho, Elias The Sparkiest

Hardware Overview

Power

Power for this board is 3.3V and we have provided multiple power options. This first and most obvious is the USB-C connector. Secondly, are the Qwiic Connectors on the left and right of the board. Thirdly, there is a 5V pin on the PTH header along the side of the board that is regulated down to 3.3V. Make sure that power you provide to this pin does not exceed 6 volts. Finally, just below the 5V pin is a 3.3V pin that should only be provided a clean 3.3V power signal.

alt text

Battery

The small metal disk in the upper right corner next to the Qwiic connector is a small lithium battery. This battery does not provide power to the IC like the 3.3V system does, but to relevant systems inside the IC that allow for a quick reconnection to satellites. The time to first fix will about ~26 seconds, but after it has a lock, that battery will allow for a two second time to first fix. This is known as a hot start and lasts for four hours after the board is powered down. The battery provides over a years worth of power to the backup system and charges slowly when the board is powered. To charge it to full, leave your module plugged in for 48 hours.

alt text

LEDs

There are four LEDs on the bottom left of the board. Starting from the left:

  • PWR: The power LED labeled as PWR will illuminate when 3.3V is activated.
  • PPS: The pulse per second LED labelled as PPS will illuminate each second once a position lock has been achieved. This generates a pulse that is synchronized with a GPS or UTC time grid. By default, you'll see one pulse a second.
  • RTK: The RTK LED will be illuminated constantly upon power up. Once RTCM data has been successfully received it will begin to blink. This is a good way to see if the ZED-F9K is getting RTCM from various sources. Once an RTK fix is obtained, the LED will turn off.
  • GEO: The GEO LED can be configured to turn on/off for geofencing applications.

alt text

Jumpers

If you flip the board over, you will notice a few jumper pads. For more information on modifying the jumpers, check out our tutorial on working with jumper pads and PCB traces.

  • I2C: This three way jumper labeled I2C connects two pull-up resistors to the I2C data lines. If you have many devices on your I2C data lines, then you may consider cutting these.
  • SPI: The jumper labeled SPI which enables the SPI data bus thus disabling the UART functions on those lines. This also disables I2C interface.
  • PWR: Starting from the right side is a jumper labeled PWR. If you cut this trace, it will disconnect the Power LED.
  • PPS: On the left of the jumper is the PPS jumper that when cut disconnects the PPS LED.
  • GEO: Cutting the GEO jumper disconnect the LED used to indicate when we reach a certain condition for geofencing applications.
  • RTK: The RTK jumper disconnects the LED used for RTK applications.

alt text

SMA Connector

The ZED-F9K requires a good quality GPS or GNSS (preferred) antenna. A SMA connector is provided for a secure connection. To get the best out of your ZED-F9K, make sure to get a GNSS multi-band antenna.

alt text

Qwiic and I2C

There are two pins labeled SDA and SCL which indicates the I2C data lines. Similarly, you can use either of the Qwiic connectors to provide power and utilize I2C. The Qwiic ecosystem is made for fast prototyping by removing the need for soldering. All you need to do is plug a Qwiic cable into the Qwiic connector and voila!

alt text

SPI

There are four pins on the right most header that are labeled with their corresponding SPI functionality. As mentioned in the jumpers section, you'll need to close the SPI jumper on the underside to enable SPI.

alt text

UART

There are two pins on the right most header currently labeled as MISO and MOSI. These are shared with the UART pins. By default, the UART interface is enabled. Be sure that the DSEL jumper on the back of the board is open.

  • TX/MISO = TX out from ZED-F9K
  • RX/MOSI = RX into ZED-F9K
Top View Bottom View
Top View Bottom View

There is a second serial port available on the ZED-F9K. This is primarily used for RTCM3 correction data. By default, this port will automatically receive and parse incoming RTCM3 strings enabling RTK mode on the board like the other RTK breakout boards for the NEO-M8P-2 and ZED-F9P. The RTCM Correction port pins are arranged to match the industry standard serial connection (aka the 'FTDI' pinout). This pinout is compatible with our Serial Basic so you can send RTCM correction data from a computer. Note that RTCM3 data can also be sent over I2C, UART1, SPI, or USB if desired.

alt text

Wheel Tick and Direction Pins

For advanced users that are interested in taking advantage of your vehicle's sensor readings, you can connect the following pins. Caution is advised however as this requires you to open up up the hood of your car and hack into the its system.

  • D-: The reference GND pin (D-) when connecting the direction pin.
  • D+: The direction pin is labeled as (D+) tells the ZED-F9K what direction the vehicle is moving (forward/reverse).
  • W-: The reference GND pin (W-) when connecting the wheel tick pin.
  • W+: The wheel tick pin (W+) tells the ZED-F9K the distance a vehicle's wheel has traveled. Depending on the odometer type that you connect to, the ZED-F9K can also receive speed data from the vehicle.

alt text

Broken Out Pins

There are four other pins broken out:

  • TXR: The transmit ready pin (TXR) enables a port to notify a device when bytes are ready to be transmitted.
  • RESET: The reset pin (RESET) resets the chip.
  • SFBT: The safeboot pin (SFBT) is used to start up the IC in safe boot mode, this could be useful if you somehow manage to corrupt the module's Flash memory.
  • INT: The interrupt pin (INT) can be used to wake the chip from power save mode.
  • PPS: The pulse per second pin (PPS) outputs pulse trains synchronized with the GPS or UTC time grid. The signal defaults to once per second but is configurable over a wide range. Read the u-blox Receiver Protocol Specification in the Resources and Going Further tab for more information.

alt text

3D IMU Orientation and Reference

For easy reference, we've documented the IMU's vectors with 3D Cartesian coordinate axes on the top and bottom side of the board. Make sure to orient and mount the board correctly so that the ZED-F9K can accurately calculate navigation information. Remember, it's all relative.

9DoF Reference (Top View) 9DoF Reference (Bottom View)
9DoF Reference (Top View) 9DoF Reference (Bottom View)

GPS Capabilities

The ZED-F9K is able to connect to up to four different GNSS constellations simultaneously with the 3D gyro and 3D accelerometer making it very accurate for its size. Below are the listed capabilities of the GPS unit.

Parameter Specification
Max navigation update rate (RTK) Priority navigation mode 30 Hz
Non-Priority navigation mode 2 Hz
Velocity Accuracy 0.05m/s
Dynamic Attitude Accuracy Heading 0.2 degrees
Pitch 0.3 degrees
Roll 0.5 degrees
Navigation Latency Priority Navigation Mode 0.5 degrees
Max Sensor Output Rate 100Hz
GNSS GPS+GLO+GAL +BDS GPS+GLO+GAL GPS+GAL GPS+GLO BDS+GLO
Time-To-First-Fix Cold Start 26s 25s 30s 25s 28s
Hot Start 2s 2s 2s 2s 2s
Aided Start 3s 3s 3s 3s 3s
Re-convergence time RTK ≤ 10s ≤ 10s ≤ 10s ≤ 10s ≤ 30s
SensitivityTracking and Navigation -160dBm -160dBm -160dBm -160dBm -160dBm
Reacquisition -157dBm -157dBm -157dBm -157dBm -157dBm
Cold Start -147dBm -147dBm -147dBm -147dBm -145dBm
Hot Start -158dBm -158dBm -158dBm -158dBm -158dBm
Position Accuracy RTK Along Track0.20m0.20m0.25m0.25m0.60m
Cross Track0.20m0.20m0.25m0.25m0.60m
2D CEP0.30m0.30m0.40m0.40m0.85m
Vertical0.30m0.30m0.40m0.40m1.00m

Performance in Different GNSS Modes from the ZED-F9K Datasheet

GNSS GPS GLONASS BeiDou Galileo
Time-To-First-Fix Cold Start 30s 28s 40s -
Hot Start 2s 2s 2s -
Aided Start 3s 3s 3s -
SensitivityTracking and Navigation -158dBm -158dBm -158dBm -156dBm
Reacquisition -157dBm -155dBm -157dBm -153dBm
Cold Start -147dBm -147dBm -141dBm -137dBm
Hot Start -158dBm -157dBm -158dBm -155dBm
Position Accuracy RTK 2D CEP0.80m1.00m-1.50m
Vertical1.00m1.50m-2.00m

Performance in Single-GNSS Modes from the ZED-F9K Datasheet

Board Dimensions

Overall, the board is about 2.00" x 1.70" (50.8mm x 43.2mm). With the USB and SMA connector, it's about 2.40" 1.70" (61.0mm x 43.2mm). There are 4x mounting holes by each corner of the board.

alt text