SparkFun GPS-RTK Dead Reckoning ZED-F9K Hookup Guide

≡ Pages
Contributors: bboyho, Elias The Sparkiest

Hardware Assembly

For this example, I used a SparkFun Thing Plus - ESP32 WROOM and associated USB cable. Connecting the boards with Qwiic cable, the assembly is very simple. Plug a Qwiic cable between the Thing Plus - ESP32 WROOM and SparkFun GPS RTK Dead Reckoning ZED-F9K. Then plug in one of our patch antennas to the SMA connector If you're going to be soldering to the through hole pins for I2C functionality, then just attach lines to power, ground, and the I2C data lines to a microcontroller of your choice.

When using the ZED-F9K, you will want to orient the board according to the guidelines explained earlier. Below is a top-down view with the board pointing up. Your setup should look similar to the image below.

alt text

Make sure to secure the board above a vehicle's dashboard using some tape or sticky tack when prototyping and testing. For best signal reception, it is suggested to guide the antenna from the inside of the car and through a window before attaching the GPS on top of a car. We recommend the magnetic mount GPS/GNSS antenna to easily mount.

alt text

Adding a RTCM Correction Source

To get the most out of the ZED-F9K you will need an RTCM correction source. There are a few methods of adding a RTCM correction source. If you have been following along with our GPS-RTK and GPS-RTK2, you can pipe correction data from a wireless network, LoRa, or cellular network. Depending on your setup, you will probably need a ZED-F9P for a correction source. For more information, check out these tutorials.

What is GPS RTK?

September 14, 2018
Learn about the latest generation of GPS and GNSS receivers to get 14mm positional accuracy!

How to Build a DIY GNSS Reference Station

October 15, 2020
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!

Setting up a Rover Base RTK System

October 14, 2020
Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.