SparkFun gator:UV Hookup Guide

≡ Pages
Contributors: santaimpersonator, Englandsaurus

Introduction

Do you have a science experiment involving weather or UV light exposure?

SparkFun gator:UV - micro:bit Accessory Board

SEN-15273
Retired

The gator:UV is the perfect tool to monitor the UV exposure in your next experiment. With the VEML6070, the gator:UV can easily be used to measure the levels of UVA (320-400 nm) radiation. This tutorial will show you how to get started using this UV sensor with the gator:bit (v2) in the micro:bit development environment.

Required Materials

To get started, you'll need a micro:bit to control everything. You can purchase one individually on in a kit.

micro:bit Board

DEV-14208
Retired

micro:bit Go Bundle

DEV-14336
Retired

SparkFun Inventor's Kit for micro:bit

KIT-15228
Retired

To easily use the gator board ecosystem, a gator:bit (v2) will help breakout the necessary pins and you will also need alligator and/or banana cables to connect the gator:bit to the gator:UV.

Alligator Test Leads - Multicolored (10 Pack)

PRT-12978
$5.25

SparkFun gator:bit v2.0 - micro:bit Carrier Board

DEV-15162
Retired

Banana to Banana Cable - Right Angle

CAB-15368
Retired

(*These banana cables have a special diameter on the attachment points designed specifically for use with the micro:bit ecosystem. They may or may not be compatible with the banana cables used on your test equipment.)

You may already have some of these materials, so feel free to modify your cart as necessary.

Suggested Reading

The gator:UV sensor is pretty straight forward to use in application. However, you may find the following concepts useful along the way.

Light

Light is a useful tool for the electrical engineer. Understanding how light relates to electronics is a fundamental skill for many projects.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

micro:climate Kit Experiment Guide

A weather station kit that is built on top of the inexpensive, easy-to-use micro:bit and Microsoft MakeCode.

If you aren't familiar with the micro:bit, we recommend reading here for an overview.

We would also recommend taking a look at the following tutorials if you aren't familiar with them.

Getting Started with the micro:bit

The BBC micro:bit is a compact, powerful programming tool that requires no software installation. Read on to learn how to use it YOUR way!

How to Load MicroPython on a Microcontroller Board

This tutorial will show you how to load the MicroPython interpreter onto a variety of development boards.

SparkFun gator:bit v2 Hookup Guide

The gator:bit v2 is a breakout board for the BBC micro:bit. The gator:bit exposes almost every pin on the micro:bit to clippable pad with circuit protection. It also has as built-in addressable LEDs and a built-in buzzer.

Hardware Overview

The gator:UV consists of 4 pads for power and data.

Contacts Direction Description
GND N/A Ground: Reference voltage and ground loop.
3.3V In Power: Provides 3.3V to sensor.
SDA Bi-directional Data: Data and commands are transmitted between the sensor and microcontroller.
SCL In Clock: The microcontroller provides the timing needed to communicate on the data line.

Power

The specified operating voltage for the VEML6070 is between 2.7V - 5.5V. For use with the gator:bit (v2) and micro:bit, you should provide 3.3V through the 3V3 and GND pads to keep the logic levels consistent.

Power Connections and LED
Power connection pads and power indication LED.

VEML6070

The VEML6070 is a UV sensor that communicates over an I2C bus. The VEML6070 detects UVA radiation up to 328 mW/cm2 with a resolution of 5 µW/cm2. For the most part, users will only need to know I2C addresses to prevent address conflicts with other devices or sensors.

VEML6070 IC
VEML6070 UV sensor.

Here are some of the characteristics of the VEML6070 sensor from the datasheet:

Characteristic Range
Operating Voltage 2.7V to 5.5V
Supply Current 240 µA
UVA Detection up to 328 mW/cm2
UVA Resolution 5 µW/cm2/step
I2C Address 0x70 - Write Commands
0x73 - Read MSB of UV Data
0x71 - Read LSB of UV Data

performance chracteristics
Performance characteristics from the datasheet. Click to enlarge.

What is UVA Radiation?

UVA radiation is a specific part of the spectrum of the solar radiation from the Sun. UVA light has wavelengths between 320 nm and 400 nm. Approximately, 4.9% of all solar radiation that makes it to the surface of the Earth is UVA light. UVA rays are often associated with photoaging and the formation of skin cancer.

solar radiation penetration through atmosphere
Penetration of solar radiation through Earth's atmosphere (from VEML6070 App. Note). Click to enlarge.

For more details on UV radiation, check out these online resources:

Some experiments and related topics for UVA radiation:

I2C Connection

I2C is a communication protocol used to transfer data between master and slave devices. It is a 2-wire connection consisting of SDA (data) and SCL (clock). The protocol is pretty well defined so it can be shared with multiple devices. This is beneficial for daisy chaining multiple devices together on a single bus. The primary thing users will need to watch out for is address conflicts (you can't have devices with the same address).

I2C Connection
I2C connection pads.

Hardware Assembly

Connecting your gator:UV to the to the gator:bit (v2) is simple. The board can also be daisy-chained with other I2C boards. This can easily be done with alligator cables or these special banana cables.

Hardware Assembly
Hardware assembly of connections used in example. Click to enlarge.
Daisy Chain
Example of daisy chaining multiple I2C gator boards. Click to enlarge.
gator:UV GND 3V3 SDA SCL
gator:bit (v2) GND 3.3V OUT P20 (SDA) P19 (SCL)

Adding the MakeCode Extension

Note: This tutorial assumes you are familiar with MakeCode, the gato:bit (v2), and the micro:bit board.

The easiest way to get started using the gator:UV is to use Microsoft MakeCode, a web-based block editor. This tutorial assumes you are familiar with the with MakeCode, the gato:bit (v2), and the micro:bit development board. If this is your first time check out this guides linked in the suggested reading section (above).

Installing Extensions

To get started with using MakeCode with the miccro:bit, head over to the MakeCode for micro:bit website by Microsoft. Then, click the New Project button to start a new project and open the Editor. (*Yes, all you only need to get start coding is a computer with internet access, an up-to-date web browser, and an available USB port!)

MakeCode Website
Click the New Project button to start a new project and open the Editor. Click on image to enlarge.

Once you have the editor up, click on the the Advanced block in the block library to reveal the drop down menu.

Editor
Click on the the Advanced block in the block library to reveal the drop down menu. Click on image to enlarge.

Finally, click on the Extensions block. This should bring up the extensions page. (*Alternatively, you could also click on the extensions link from the settings menu.)

Advanced Block
Click on the the Extensions block to open the extensions page. Click on image to enlarge.

There are two methods for finding the gator:UV extension:

  • Search for the name used on the extension1.
  • Use the link to the GitHub repository for the pxt-package as the search term.

Extensions Page
Use the search bar to find the extension you want to install. Click on image to enlarge.

Note: Unfortunately, it does take time to get an extension approved by the micro:bit Educational Foundation before it can be searchable by name. Part of the requirements for the approval process involves a live product page. Therefore, at the time of the launch of this product, the extension has not been approved yet and the only method of adding the extension is to use the link to the GitHub repository of the pxt-package. We will update this tutorial as soon as the extension has been approved.↩

Search for the PXT-Package

Search for the gator:UV extension using the GitHub repository link to the pxt-package:

https://github.com/sparkfun/pxt-gator-UV

Search for Extension
Search for Extension. Then, click on the box to add it to the block library. Click on image to enlarge.

Then, click on the box for the extension to add it to the block library. The gator:UV extension should now appear in the block library.

Extension in Block Library
Extension in the block library; click on the block to open menu options. Click on image to enlarge.

To verify that you have added the extension, click on the gator:UV block to make sure that your drop down menu options match the image below.

Menu Options
Available blocks for the gator:UV extension. Click on image to enlarge.

MakeCode Examples

Now that you have added the gator:particle extension to the Editor, lets start with some example code. Plug the micro:bit into your computer using an USB micro-B cable after you have assembled your hardware with the instructions from the previous section. The micro:bit should appear on your computer as a removable storage device.

USB Drive
The micro:bit showing up as a USB drive on a Windows computer. Click to enlarge.

To upload new code, this is where you will be copying the downloaded .hex file to later.

Block Functions

Initialize gator:UV sensor
This block should be pretty self explanatory, it sets the sensor up to be used. You should use this within the on start block.

get UVA Reading
This is a value block as indicated by the block's shape. The output of the block is value measured by the UV sensor.

  • 0 to 65535- A 16-bit value of the UV sensor reading that can be correlated to the UV-Index.

set refresh time on UV Sensor to _____
This sets the integration time for the UV sensor. The refresh time should be adjusted for the range of values you expect to be measuring.

  • half- Half of the normal integration time.
  • one- Normal integration time (default).
  • two- Twice the normal integration time.
  • four-Four times the normal integration time.

Note: *Although not exactly correct, it can be interpreted as the time that the sensor spends collecting a data sample.

If you are barely measuring changes between measurement values, you should try to increase the refresh time, which allows the sensor to collect more light. The relation between measured values and the reset time are linear (see table below).

UV Index

The table below maps out UV index to the correlating sensor output values and their respective refresh time (or integration time) setting. The values were extrapolated from the UV index tables provided in the VEML6070 Application Note for an RSET = 300kΩ.

Int. Time = x0.5 Int. Time = x1 Int. Time = x2 Int. Time = x4 UVI (Value) UV-INDEX
≥ 1142 ≥ 2283 ≥ 4565 ≥ 9130 ≥ 11 Extreme
831 to 1141 1661 to 2282 3321 to 4464 6641 to 9129 8 to 10 Very High
623 to 830 1246 to 1660 2491 to 3320 4981 to 6640 6,7 High
312 to 622 623 to 1245 1245 to 2490 2490 to4980 3 to 5 Moderate
0 to 311 0 to 622 0 to 1244 0 to 2489 0 to 2 Low

Basic Reading

Below, is a simple example of how to take simple measurements from the sensor. To use this example, there are multiple options for accessing the .hex file:

  • Replicate the block functions from the display below to copy the example project. Then download the .hex file.
  • Expand the display widow to pull up the example project. Then download the .hex file.
  • Use this link to pull up the example project. Then download the .hex file.
  • Download the .hex file from the button below or the link on the bottom of the display.

The output is redirected over the serial port to avoid conflicts on pins P0 and P1, which are also used for serial communication. To read the sensor values, pull up your favorite serial terminal emulator. Then, connect to the serial port that the micro:bit is on; the default baud rate is 115200 bps. Below, is an example of the sensor output for the example code (the sensor values are responding to the flashlight on my phone).

Sample Readings
Example of readings from the sensor.

Do Not Try This at Home: In case you were thinking about it, do NOT try to replicate this image or attempt to max out your readings with a magnifying glass. You will burn or damaged the board. I had the magnifying glass focused on the board for less than a second for this picture and it started to burn and smolder.

Magnifying Glass

Troubleshooting the Extension

To manually install this extension in makecode, go to the "Extensions" tab on the left side of the makecode site:

alt text

In the location you'd normally search for an extension, you'll notice an upload button on the right:

alt text

Click on this, and you'll get a window allowing you to upload your own built extension. Navigate to where you saved the above extension hex, and upload it to your project.

alt text

You should be able to see the extension and its functions now. In addition, you'll be able to build and download your project to your variant of micro:bit.

alt text

Other Troubleshooting Tips

Power and Connections

Check that your power and data connections are correct and that the power VOUT switch is in the ON position on the gator:bit (v2).

UV Filters

Make sure that if you are using a transparent cover over the sensor that it still passes UV light. More modern clear plastics and glass covers (especially for photo or documents) usually have a special UV coating to prevent pigment deterioration and yellowing of paper.

If you still have questions or issues with this product, please create a post on our forum under the Gator Products topic.

Additionally, if you are an educator and you have class or application based questions, please create a post on our forum under the Educational Products topic.

Resources and Going Further

For more product information, check out the resources below:

Interested in the micro:bit? Check out some of these other micro:bit products:

SparkFun Inventor's Kit for micro:bit v2 Lab Pack

LAB-17363
$460.00

micro:bit v2 Club Kit - Go Bundle 10-Pack

KIT-17290
$199.95

SparkFun Inventor's Kit for micro:bit v2

KIT-17362
$53.50

micro:bit v2 Board

DEV-17287
$16.50

Need some inspiration for your next project? Check out some of these other micro:bit product tutorials:

Gator:color ProtoSnap Hookup Guide

Clip some LED's onto your gator:bit with the gator:color.

SparkFun gator:particle Hookup Guide

The gator:particle is an I2C heart-rate monitor and pulse oximeter that can be used as a particle sensor. This tutorial will get you started using the gator:particle with the micro:bit platform.

SparkFun gator:RTC Hookup Guide

The gator:RTC is an I2C based, real-time clock (RTC) for keeping time while your micro:bit isn't powered. This tutorial will get you started using the gator:RTC with the micro:bit platform.

SparkFun gator:log Hookup Guide

The gator:log is a serial communication based data logger. This tutorial will get you started using the gator:log with the micro:bit platform.