SparkFun gator:UV Hookup Guide

≡ Pages
Contributors: santaimpersonator, Englandsaurus

Adding the MakeCode Extension

Note: This tutorial assumes you are familiar with MakeCode, the gato:bit (v2), and the micro:bit board.

The easiest way to get started using the gator:UV is to use Microsoft MakeCode, a web-based block editor. This tutorial assumes you are familiar with the with MakeCode, the gato:bit (v2), and the micro:bit development board. If this is your first time check out this guides linked in the suggested reading section (above).

Installing Extensions

To get started with using MakeCode with the miccro:bit, head over to the MakeCode for micro:bit website by Microsoft. Then, click the New Project button to start a new project and open the Editor. (*Yes, all you only need to get start coding is a computer with internet access, an up-to-date web browser, and an available USB port!)

MakeCode Website
Click the New Project button to start a new project and open the Editor. Click on image to enlarge.

Once you have the editor up, click on the the Advanced block in the block library to reveal the drop down menu.

Editor
Click on the the Advanced block in the block library to reveal the drop down menu. Click on image to enlarge.

Finally, click on the Extensions block. This should bring up the extensions page. (*Alternatively, you could also click on the extensions link from the settings menu.)

Advanced Block
Click on the the Extensions block to open the extensions page. Click on image to enlarge.

There are two methods for finding the gator:UV extension:

  • Search for the name used on the extension1.
  • Use the link to the GitHub repository for the pxt-package as the search term.

Extensions Page
Use the search bar to find the extension you want to install. Click on image to enlarge.

Note: Unfortunately, it does take time to get an extension approved by the micro:bit Educational Foundation before it can be searchable by name. Part of the requirements for the approval process involves a live product page. Therefore, at the time of the launch of this product, the extension has not been approved yet and the only method of adding the extension is to use the link to the GitHub repository of the pxt-package. We will update this tutorial as soon as the extension has been approved.↩

Search for the PXT-Package

Search for the gator:UV extension using the GitHub repository link to the pxt-package:

https://github.com/sparkfun/pxt-gator-UV

Search for Extension
Search for Extension. Then, click on the box to add it to the block library. Click on image to enlarge.

Then, click on the box for the extension to add it to the block library. The gator:UV extension should now appear in the block library.

Extension in Block Library
Extension in the block library; click on the block to open menu options. Click on image to enlarge.

To verify that you have added the extension, click on the gator:UV block to make sure that your drop down menu options match the image below.

Menu Options
Available blocks for the gator:UV extension. Click on image to enlarge.