Sparcade: Edison as a Web Server for Browser Games

≡ Pages
Contributors: Shawn Hymel

Resources and Going Further

To connect the Edison to the internet, connect via SSH and run the command:

configure_edison --WiFi

Follow the instructions to connect to a WiFi AP. Additionally, you can start running the Edison's default web server again with:

systemctl enable edison_config.service
reboot

Note that you may want to load a different program via XDK so that the custom server does not continue to run on boot.

What other games can you make? To learn about how Vortex was made, check out the Phaser.io framework. Controlling hardware (specifically, the LCD) from the Edison is accomplished using the Johnny-Five platform.

All the resources used in this tutorial can be found below.

For more Intel® Edison fun, check out the following tutorials:

Loading Debian (Ubilinux) on the Edison

How to load a Debian distribution (specifically Ubilinux) onto the Edison.

Using an LCD on the Edison

How to connect an LCD controlled by an ILI9341 driver to the IntelĀ® Edison.

Interactive Smart Mirror

Build a smart mirror that displays weather data using the IntelĀ® Edison.