Comments: Soil Moisture Sensor Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #1899296 / about 2 years ago / 1

    Can the contacts that reach the soil be soldered onto? I would like to run some remote contacts to this sensor, but wondering if there are separate provisions or I can solder to the contacts to do this? Thanks!

  • Member #1480738 / about 8 years ago / 1

    Hi. Why does this tutorial recommend "powering the ... Moisture Sensor ... between 3.3V - 5V", but then the battery recommended is 9V. Is that going to be ok? If so, why?

  • Member #1480738 / about 8 years ago / 1

    Why is there a breadboard? I appear to successfully get readings using just the red USB cord, the arduino redboard, the 3 wires (red, yellow, black) and the soil moisture sensor. Am I missing something important by not using the breadboard?

    • santaimpersonator / about 7 years ago / 1

      The breadboard was originally used for the LCD screen. The screen was updated in the last year or so; now, you don't need as many wires. However, the breadboard was still included in the list for customers who may want to use it.

  • Member #1480738 / about 8 years ago / 1

    hi i'm looking at the photo: https://cdn.sparkfun.com/assets/learn_tutorials/3/9/0/Soil_Moisture_Sensor_Hook_Up_Guide-02.jpg

    with the red, yellow and black wire going into the sensor - but they don't stick in there (they do stick into the breadboard) - does that mean i need to melt the tips of the red,yellow,black wires to stay into the moisture sensor holes?

    • Member #1480738 / about 8 years ago / 1

      oh, i get it. i needed to buy an extremely small screw driver and pinch the tip of the wire inside the sensor by tightening the screw.

  • Member #737950 / about 9 years ago / 1

    How best to locate these sensors 15 to 20 feet away from the Arduino? One of your pictures shows 3-strand twisted wire, which looks like a great solution - but I can't find it for sale on Sparkfun. Thanks!

    • santaimpersonator / about 7 years ago / 1

      Hi there, it sounds like you are looking for technical assistance. Please use the link in the banner above, to get started with posting a topic in our forums. Our technical support team will do their best to assist you.

      That is just some wire that was hand twisted for the demo. We don't currently carry twisted/braided wire like that. However, you can probably look for some low voltage wire from your local hardware store. Just be aware that wire has its own internal resistance. Therefore, you may run into voltage drop issues the further away the sensor is.

  • thomthom / about 9 years ago / 1

    When using digital out to power the sensor with an Arduino, do you need some amount of delay from setting the digital out high before you read the analog in?

    • santaimpersonator / about 7 years ago / 1

      Hi there, it sounds like you are looking for technical assistance. Please use the link in the banner above, to get started with posting a topic in our forums. Our technical support team will do their best to assist you.

      The pin just needs to be high while you are taking a reading. You may want to give the sensor a split second to settle though.

  • Member #727140 / about 9 years ago / 1

    Nicely done but unless I missed something what about just using a small solenoid valve? Example: Adafruit Plastic Water Solenoid Valve - 12V - 1/2" Nominal PRODUCT ID: 997 $6.95 The creativity is great but it seems like once the cost of all of the mechanical parts are added up and given that none of the motors and parts were designed to be around water the approach seems questionable as a long term solution. Think corrosion and mineral deposits and short circuits.

    Not trying to rain on your parade because I think creative solutions are cool but I had to ask.

  • Member #900083 / about 10 years ago / 1

    Hi! I have two students working on this project and they love it. They are having trouble with the lcd connection and unfortunately, my knowledge base does not allow me to help, I'm learning along with them. Any chance you have a schematic or photo of the breadboard setup with just the moisture sensor and lcd screen? They are leaving out the pump for now.

    • santaimpersonator / about 7 years ago / 1

      Hi there, it sounds like you are looking for technical assistance. Please use the link in the banner above, to get started with posting a topic in our forums. Our technical support team will do their best to assist you.

  • Member #825006 / about 10 years ago * / 1

    Hello. I am a Year 10 student working on this for a project but I am having troubles setting up a watering system. I've read the guide and comments below but I still don't quite understand the watering setup. Also, I do not have access to all the part you mentioned in the guide for the watering part, just some simple gears and motor. My idea was to have a plastic tube come down from a container of water and rest against a gear which is connected to the motor. The gear has holes so that when it turns and the plastic tube goes over the holes, the water in the plastic tube is let through. When the plastic tube is not over any holes, the water is blocked. My problem is how do I set it up so that the tube is firmly pressed against the gear so that water won't leak but still be able allow the gear to turn. Also, recommendations of other ways to set up the water system would be great! Thank you for reading!

    • santaimpersonator / about 7 years ago / 1

      Hi there, it sounds like you are looking for technical assistance. Please use the link in the banner above, to get started with posting a topic in our forums. Our technical support team will do their best to assist you. Just be aware that we primarily assist with our products; we may not be able to help with your mechanical setup.

  • Member #802861 / about 10 years ago * / 1

    Hey! I just started experimenting with the soil moisture sensor, but am having some problems with the readings. Basically if I stick it into water it generates a reading of about 580, and if I take it out the reading is about 280. After sticking it into very dry soil I still get a bouncy reading between 520 and 560. Are these reading accurate? Is there maybe some documentations that I could look at? I read through all of the links provided, but cant seem to find a more accurate guide on this...

    Also, do you recommend using any resistors? I saw in the schematics that a 10k resistor can be used...any suggestions on that?

    EDIT:

    I also used this to check voltage readings: float getVoltage(int pin) { return (analogRead(pin) * 0.004882814); }

    Voltage is always around 3.8....

    Thanks and have a great day! Urban

    • santaimpersonator / about 7 years ago / 1

      Hi there, it sounds like you are looking for technical assistance. Please use the link in the banner above, to get started with posting a topic in our forums. Our technical support team will do their best to assist you.

      The value read on SIG is dependent on the power input, soil composition, and will vary with the moisture content of the soil. For example, if you have a high alkaline content in your soil, it will be more conducive and give you a high baseline reading. There is some information in the Calibration section to get you started; however, it is up to the user to analyze the readings for their needs.

    • Joel_E_B / about 10 years ago / 1

      Hi, those readings don't sound correct. The sensor should be reading close to zero when completely dry and close to the maximum value of your ADC (ie 1023 for a 10-bit resolution) when submersed in water. Are you powering the sensor with 5V? Why are you multiplying the reading by the decimal value above?

  • Member #796279 / about 11 years ago / 1

    Could you please explain how this motor watering pump / thingy is supposed to work? All I can see is two photos, a parts list and some code, but no assembly instructions, no diagram, movie, text or anything that describes the working principle.

    • Sarah Al-Mutlaq / about 11 years ago / 2

      Of course! The way I set it up was with a bucket above connected to a crazy straw, that was secured to a laser cut piece (with water tight glue). This piece had a hole where the straw was and fit inside the gear that the motor was rotating, The hole was small enough that a drop would be let out when the holes from the gear came around, making a make sift watering system. The lasers cut piece was secured with an o ring to keep everything water tight. Hope that helps. It was a quick project, and there are better solutions out there.

  • Member #415908 / about 11 years ago / 1

    What values are the resistors on this sensor ( I assume they form a voltage divider)? Other than the resistors, the two leads are pretty much it?

  • Member #756451 / about 11 years ago / 1

    Good tutorial. How can I make the data to be sent to a screen that is not wired to the microcontroller hosting the sensor? Thanks, Luis G

    • Sarah Al-Mutlaq / about 11 years ago / 1

      You could do this with some Bluetooth boards, sending data wirelessly that way, we have a great tutorial to get you started with that Here. You could also use Wifi, and Here is a good tutorial on getting started with that. There are also lots of other ways that you could get creative, so I would look into wireless technology it's all pretty cool! I hope that answers you question and helps you a little!

  • MTMentat / about 11 years ago / 1

    What type/chemistry/brand of conformal coating did you guys use, if you don't mind sharing?

    • Joel_E_B / about 11 years ago / 2

      We bought a bottle of this for around the office, and have been using it on everything we can since.

    • MTMentat / about 11 years ago / 1

      Thanks, Joel! That's pretty much what I figured, and having ordered it I'm looking forward to protecting my circuits in harsher-than-benchtop environments in the future!

  • To make it a little easier to connect, you could also use the JST to Breadboard Jumper (3-pin) https://www.sparkfun.com/products/13685 with the 3 pin JST connector https://www.sparkfun.com/products/9750 with the soil moisture sensor and serial enabled LCD.


If you've found an issue with this tutorial content, please send us your feedback!