smôl ARTIC R2 Hookup Guide

≡ Pages
Contributors: PaulZC

Hardware Overview

In this section we'll cover what's included on the smôl ARTIC R2 Peripheral Board.

ARTIC R2

The heart of the smôl ARTIC R2 is, of course, the ARTIC R2 transceiver itself. This is a clever chip containing a Digital Signal Processor (DSP) which modulates transmit messages and demodulates received messages. The DSP can boot from on-board flash memory or from an external microcontroller via SPI. When transmitting, it produces a 1mW (0dBm) output signal which is fed to a separate power amplifier.

Pictured is the ARTIC R2 chip

Our Arduino Library does all of the heavy lifting for you. By default, the library will tell the ARTIC R2 DSP to boot from the on-board flash memory. However, by changing one line of code, you can instead boot via SPI with your microcontroller providing the firmware for the DSP.

RF Amplifier

During transmit, the RFPA0133 power amplifier boosts the 0dBm (1mW) signal from the ARTIC R2.

Pictured is the RFPA0133 amplifier chip

By default, the amplifier uses full gain and boosts the signal to approximately 25.8dBm (380mW). If you are using ARGOS 2 or 3 modulation and are transmitting from a 'noisy' environment, like a city, then you are probably going to need to use full power to ensure your messages get through. However, if you are using ARGOS 4 modulation and/or are transmitting from a 'quiet' environment, like the tundra or the ocean, then you will be able to transmit at reduced power.

Gain Control

There are two ways to reduce the smôl ARTIC R2 transmit power. You can adjust the gain through software and the on-board opto-isolated gain control circuit.

Pictured is the opto-isolated gain control

Our Arduino Library can reduce the gain for you. If you call:

language:c
myARTIC.attenuateTXgain(true);

from inside your code, the opto-isolator will pull the RFPA0133's G8 pin low, reducing the gain by approximately 5dB. This also has the advantage of reducing the transmit current by approximately 80mA.

If you are experimenting with ARGOS 4 modulation, you may want to reduce the gain even further. You can do that by opening the split-pad jumper next to the opto-isolator. Opening the jumper will pull the RFPA0133's G16 pin low and will reduce the gain by approximately 11dB. If you haven't used jumpers before, please check out our tutorial.

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

Flash Memory

If you turn the smôl ARTIC R2 over, you will be able to see the small flash memory chip.

Pictured is the flash memory chip

During production testing at SparkFun, we program the flash memory with the ARTIC R2 firmware (ARTIC006) and a Platform ID allocated by CLS. You will need to register the Platform ID on your ARGOS account to activate it.

GPIO Expander

The larger chip on the bottom of the board is a PCA9536 I2C GPIO expander.

Pictured is the PCA9536 GPIO expander

smôl only supports two GPIO signals, so we added a separate I2C GPIO expander to allow the ARTIC R2 RESETB, INT1 and BOOT signals, plus the RF amplifier G8 pin, to be controlled via I2C.

You won't need to communicate with the GPIO expander directly, our Arduino Library will do that for you, we're just letting you know why that chip is there.

Antenna

The antenna connection for the ARTIC R2 is u.FL.

Pictured is the u dot f l antenna connector

Check out our tutorial if you haven't used u.FL before:

Three Quick Tips About Using U.FL

Quick tips regarding how to connect, protect, and disconnect U.FL connectors.

Warning: Always connect a 401MHz antenna to your smôl ARTIC R2 before connecting the power. Transmitting with no antenna attached will damage the RF power amplifier.

FPC Connections

Like all of our smôl boards, the ARTIC R2 Peripheral Board is equipped with two 16-way 0.5mm-pitch Flexible Printed Circuit connectors. FPCs are used to link the smôl boards together in a daisy-chain.

The pin-out for the smôl ARTIC R2 IN connector is as follows:

IN Connector Pin No.Signal NameFunctionNotes
1PROC_PWR_ENProcessor Power EnableNot used
23V33.3V Power Rail
3GNDPower Ground / 0V
4SCLKSPI ClockUsed to communicate with the ARTIC R2
5COPISPI Controller Out Peripheral InUsed to communicate with the ARTIC R2
6CIPOSPI Controller In Peripheral OutUsed to communicate with the ARTIC R2
7CS0SPI Chip Select 0Used to communicate with the ARTIC R2
8CS1SPI Chip Select 1Connected to Pin 7 (CS0) on the OUT connector
9CS2SPI Chip Select 2Connected to Pin 8 (CS1) on the OUT connector
10GPIO0Power ControlPull high to enable power for the ARTIC R2
11GPIO1General Purpose Input / Output 1Connected to Pin 10 (GPIO0) on the OUT connector
12SDAI2C DataUsed to communicate with the PCA9536 GPIO expander
13SCLI2C ClockUsed to communicate with the PCA9536 GPIO expander
14GNDPower Ground / 0V
153V33.3V Power Rail
16V_USBUSB Power Rail (5V)Not used

The pin-out for the smôl ARTIC R2 OUT connector is as follows:

OUT Connector Pin No.Signal NameFunctionNotes
1PROC_PWR_ENProcessor Power EnableNot used
23V33.3V Power Rail
3GNDPower Ground / 0V
4SCLKSPI ClockUsed to communicate with the ARTIC R2
5COPISPI Controller Out Peripheral InUsed to communicate with the ARTIC R2
6CIPOSPI Controller In Peripheral OutUsed to communicate with the ARTIC R2
7CS0SPI Chip Select 0Connected to Pin 8 (CS1) on the IN connector
8CS1SPI Chip Select 1Connected to Pin 9 (CS2) on the IN connector
9CS2SPI Chip Select 2Not connected
10GPIO0General Purpose Input / Output 0Connected to Pin 11 (GPIO1) on the IN connector
11GPIO1Not connected
12SDAI2C DataUsed to communicate with the PCA9536 GPIO expander
13SCLI2C ClockUsed to communicate with the PCA9536 GPIO expander
14GNDPower Ground / 0V
153V33.3V Power Rail
16V_USBUSB Power Rail (5V)Not used

We use a technique called waterfalling on the CS and GPIO signals. If you haven't used waterfalling before, please check out the smôl Hookup Guide.