Secure DIY Garage Door Opener

≡ Pages
Contributors: QCPete

Power Considerations

In order to save power on the remote control, I opted to put a momentary push button in series on the power input. This way, power would only be connected when I wanted to open the garage door. Otherwise, it would remain completely off. Also, with a more traditional DPST switch, we'd be more likely to accidentally leave it switched on and drain the battery. Luckily, the ProRF has a couple headers already in the design for an external switch.

alt text

These switch headers made it easy to integrate the momentary power switch.

Now I wanted to consider how much power is actually being used during each attempt to open the garage door. I hooked up an SparkFun RedBoard Artemis and a Zio Current and Voltage Sensor - INA219 (Qwiic), and I had some data streaming in no time!

alt text

The Zio qwiic current setup to measure current draw on the system.

Here is what a complete cycle looked like on the serial plotter and monitor:

alt text

Serial plotter showing the current used during a complete cycle.

Each reading is precisely 100ms apart, so adding them all up I can see that it will use 0.065mAh per cycle.

21 readings (2100ms) at 36mA = 0.021mAh

1 reading (100ms) at 56mA = 0.002mAh

20 readings (2000ms) at 76mA = 0.042mAh

Total: 0.065mAh

Battery capacity is 400mAh

400mAh / 0.065mAh = 6,153

So according to my rough math, I think I can press this button 6153 times with this single battery. At 2 times a day, 300 days a year (600/year), that's 10 years. Even with capacity loss during storage in my car (let's say 10% each year), it'll still should last... let's see...

Year: capacity : -10% - yearly use for cycles (600 * 0.065 = ~40mAh)

Year 1 : 400 - 40 - 40 = 320

Year 2 : 320 - 32 - 40 = 248

Year 3 : 248 - 25 - 40 = 183

Year 4 : 183 - 18 - 40 = 125

Year 5 : 125 - 13 - 40 = 72

Year 6 : 72 - 7 - 40 = 25

Wahoo! Six years is pretty good. Now I just need to make sure it doesn't get squashed somewhere in my car.