Secure DIY Garage Door Opener

≡ Pages
Contributors: QCPete

Arduino Code

There are two separate sketches: one for the remote control and a second for the base transceiver. You can see both sketches in the project GitHub repository located here:

The code used in this project was kept fairly clean by using three Arduino Libraries:

For help with installing each necessary Arduino library, see the individual hookup guides for the Qwiic Relay and Cryptographic Co-processor. But you can also check out a more general tutorial on Arduino library installation here:

Installing an Arduino Library

January 11, 2013
How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Also, to use the SparkFun Pro RF, you will need to install the SAMD board packages. For more information on how to do that, you can take a look at this section of the Pro RF Hookup Guide. Now let's take a closer look at each individual sketch.

Remote Control Sketch

This sketch basically does everything inside its setup(). This is because, it will actually remain un-powered for most of its life. When I want to power it up and begin an entire attempt cycle, I will press the momentary button on the enclosure and this will supply power.

After setting up the RF module, the cryptographic co-processor and button, the most important thing to note is that it calls "attempt_cycle" at the very end of setup(). All the good stuff happens in there!

The attempt_cycle() function does essentially four things:

  • Engages a cycle by sending "$$$".
  • Receives 64-byte token.
  • Creates the ECC signature.
  • Sends Signature back to the base.

language:c
    /*
  Remote Control
  This sketch is used to create a cryptographically secure wireless controller to open you garage.
  The complete system uses SparkFun Pro RF modules, Cryptographic Co-processors, and the qwiic relay.
  Note, it also requires a base transceiver setup with separate sketch.

  See the complete tutorial here:
  https://learn.sparkfun.com/tutorials/secure-diy-garage-door-opener

  By: Pete Lewis
  SparkFun Electronics
  Date: January 13th, 2020
  License: This code is public domain but you can buy me a beer if you use this and we meet someday (Beerware license).

  Feel like supporting our work? Please buy a board from SparkFun!
  https://www.sparkfun.com/products/15573

  Some of this code is a modified version of the example provided by the Radio Head
  Library which can be found here:
  www.github.com/PaulStoffregen/RadioHeadd

  Some of this code is a modified version of the example provided by the SparkFun ATECCX08a
  Arduino Library which can be found here:
  https://github.com/sparkfun/SparkFun_ATECCX08a_Arduino_Library
*/

#include <SPI.h>

//Radio Head Library:
#include <RH_RF95.h>

// We need to provide the RFM95 module's chip select and interrupt pins to the
// rf95 instance below.On the SparkFun ProRF those pins are 12 and 6 respectively.
RH_RF95 rf95(12, 6);

int LED = 13; //Status LED is on pin 13

int packetCounter = 0; //Counts the number of packets sent
long timeSinceLastPacket = 0; //Tracks the time stamp of last packet received

// The broadcast frequency is set to 921.2, but the SADM21 ProRf operates
// anywhere in the range of 902-928MHz in the Americas.
// Europe operates in the frequencies 863-870, center frequency at 868MHz.
// This works but it is unknown how well the radio configures to this frequency:
//float frequency = 864.1;
float frequency = 921.2; //Broadcast frequency


//////////////crypto stuff

#include <SparkFun_ATECCX08a_Arduino_Library.h> //Click here to get the library: http://librarymanager/All#SparkFun_ATECCX08a
#include <Wire.h>

ATECCX08A atecc;

uint8_t token[32]; // time to live token, created randomly each authentication event


/////////////

byte buf[RH_RF95_MAX_MESSAGE_LEN];

void setup()
{
  pinMode(LED, OUTPUT);

  SerialUSB.begin(115200);
  // It may be difficult to read serial messages on startup. The following line
  // will wait for serial to be ready before continuing. Comment out if not needed.
  //while (!SerialUSB);
  SerialUSB.println("RFM Client!");

  //Initialize the Radio.
  if (rf95.init() == false) {
    SerialUSB.println("Radio Init Failed - Freezing");
    while (1);
  }
  else {
    //An LED inidicator to let us know radio initialization has completed.
    //SerialUSB.println("Transmitter up!");
    //digitalWrite(LED, HIGH);
    //delay(500);
    //digitalWrite(LED, LOW);
    //delay(500);
  }

  // Set frequency
  rf95.setFrequency(frequency);

  // The default transmitter power is 13dBm, using PA_BOOST.
  // If you are using RFM95/96/97/98 modules which uses the PA_BOOST transmitter pin, then
  // you can set transmitter powers from 5 to 23 dBm:
  // Transmitter power can range from 14-20dbm.
  rf95.setTxPower(14, false);

  pinMode(5, INPUT_PULLUP);

  Wire.begin();

  if (atecc.begin() == true)
  {
    SerialUSB.println("Successful wakeUp(). I2C connections are good.");
  }
  else
  {
    SerialUSB.println("Device not found. Check wiring.");
    while (1); // stall out forever
  }

  attempt_cycle();

}


void loop()
{

  if (digitalRead(5) == LOW)
  {
//    attempt_cycle();
  }
  delay(10); // button debounce
}


void printBuf64()
{
  SerialUSB.println();
  SerialUSB.println("uint8_t buf[64] = {");
  for (int i = 0; i < 32 ; i++)
  {
    SerialUSB.print("0x");
    if ((buf[i] >> 4) == 0) SerialUSB.print("0"); // print preceeding high nibble if it's zero
    SerialUSB.print(buf[i], HEX);
    if (i != 31) SerialUSB.print(", ");
    if ((31 - i) % 16 == 0) SerialUSB.println();
  }
  SerialUSB.println("};");
  SerialUSB.println();
}

void printToken()
{
  SerialUSB.println();
  SerialUSB.println("uint8_t token[32] = {");
  for (int i = 0; i < sizeof(token) ; i++)
  {
    SerialUSB.print("0x");
    if ((token[i] >> 4) == 0) SerialUSB.print("0"); // print preceeding high nibble if it's zero
    SerialUSB.print(token[i], HEX);
    if (i != 31) SerialUSB.print(", ");
    if ((31 - i) % 16 == 0) SerialUSB.println();
  }
  SerialUSB.println("};");
  SerialUSB.println();
}


// Note, in Example4_Alice we are printing the signature we JUST created,
// and it lives inside the library as a public array called "atecc.signature"
void printSignature()
{
  SerialUSB.println("uint8_t signature[64] = {");
  for (int i = 0; i < sizeof(atecc.signature) ; i++)
  {
    SerialUSB.print("0x");
    if ((atecc.signature[i] >> 4) == 0) SerialUSB.print("0"); // print preceeding high nibble if it's zero
    SerialUSB.print(atecc.signature[i], HEX);
    if (i != 63) SerialUSB.print(", ");
    if ((63 - i) % 16 == 0) SerialUSB.println();
  }
  SerialUSB.println("};");
  SerialUSB.println();
}

void attempt_cycle()
{
  SerialUSB.println("Sending message");

  //Send a message to the other radio
  uint8_t toSend[] = "$$$";
  //sprintf(toSend, "Hi, my counter is: %d", packetCounter++);
  rf95.send(toSend, sizeof(toSend));
  rf95.waitPacketSent();

  // Now wait for a reply

  byte len = sizeof(buf);

  if (rf95.waitAvailableTimeout(2000)) {
    // Should be a reply message for us now
    if (rf95.recv(buf, &len)) {
      SerialUSB.print("Got reply: ");
      printBuf64();
      for (int i = 0 ; i < 32 ; i++) token[i] = buf[i]; // read in token from buffer.
      printToken(); // nice debug to see what token we just sent. see function below

      boolean sigStat = false;
      sigStat = atecc.createSignature(token); // by default, this uses the private key securely stored and locked in slot 0.

      SerialUSB.print("sigStat: ");
      SerialUSB.println(sigStat);

      //printSignature();


      // Copy our signature from library array to local toSend array
      //for (int i = 0 ; i < 64 ; i++) toSend[i] = atecc.signature[i]; // store locally

      //Send signature to the other radio
      rf95.send(atecc.signature, sizeof(atecc.signature));
      rf95.waitPacketSent();
      SerialUSB.println("Sent signature");
      //SerialUSB.println((char*)buf);
      //SerialUSB.print(" RSSI: ");
      //SerialUSB.print(rf95.lastRssi(), DEC);
    }
    else {
      SerialUSB.println("Receive failed");
    }
  }
  else {
    SerialUSB.println("No reply, is the receiver running?");
  }
  delay(500);
}

Base Transceiver Sketch

This sketch is very similar to the first Example Sketch in our hookup guide for the Pro RF: Point to Point Radio Arduino Examples. In fact, that's were I started from. And then I added in the necessary libraries for the Cryptographic chip and the Qwiic relay. And then I stole some code from each of their initial examples. A whole lot of copy/paste going on. Isn't that convenient, Gromit!

Inside the main loop, the Base does the following:

  • Listens to incoming messages.
  • If it receives a "$$$", then create a new random token and send it to remote.
  • Listens for a signature from remote.
  • Receives 64-byte signature.
  • Verifies signature.
  • If valid, trigger relay to "close" for 500ms, emulating a button press.
  • If success hasn't happened within 1 second, destroy token. This protects against repeater attacks.

Note, whenever the Base hears any message come in, it checks for the "$$$". This will tell it if the message is an request or a signature. If it doesn't see "$$$" then it pulls in the next 64 bytes and attempts to verify the signature.

language:c
/*
  Base Transceiver
  This sketch is used to create a cryptographically secure wireless controller to open you garage.
  The complete system uses SparkFun Pro RF modules, Cryptographic Co-processors, and the qwiic relay.
  Note, it also requires a remote control setup with separate sketch.

  See the complete tutorial here:
  https://learn.sparkfun.com/tutorials/secure-diy-garage-door-opener

  By: Pete Lewis
  SparkFun Electronics
  Date: January 13th, 2020
  License: This code is public domain but you can buy me a beer if you use this and we meet someday (Beerware license).

  Feel like supporting our work? Please buy a board from SparkFun!
  https://www.sparkfun.com/products/15573

  Some of this code is a modified version of the example provided by the Radio Head
  Library which can be found here:
  www.github.com/PaulStoffregen/RadioHeadd

  Some of this code is a modified version of the example provided by the SparkFun ATECCX08a
  Arduino Library which can be found here:
  https://github.com/sparkfun/SparkFun_ATECCX08a_Arduino_Library

  Some of the code is a modified version of the example provided by the SparkFun Qwiic
  Relay Arduino Library which can be found here:
  https://github.com/sparkfun/SparkFun_Qwiic_Relay_Arduino_Library
*/



#include <SPI.h>

//Radio Head Library:
#include <RH_RF95.h>

// We need to provide the RFM95 module's chip select and interrupt pins to the
// rf95 instance below.On the SparkFun ProRF those pins are 12 and 6 respectively.
RH_RF95 rf95(12, 6);

int LED = 13; //Status LED on pin 13

int successLED = 3; // green
int failLED = 4; // red
int statLED = 2; // blue

int packetCounter = 0; //Counts the number of packets sent
long timeSinceLastPacket = 0; //Tracks the time stamp of last packet received
// The broadcast frequency is set to 921.2, but the SADM21 ProRf operates
// anywhere in the range of 902-928MHz in the Americas.
// Europe operates in the frequencies 863-870, center frequency at
// 868MHz.This works but it is unknown how well the radio configures to this frequency:
//float frequency = 864.1;
float frequency = 921.2;

uint8_t buf[RH_RF95_MAX_MESSAGE_LEN];


////////////////relay

#include "SparkFun_Qwiic_Relay.h"

#define RELAY_ADDR 0x18 // Alternate address 0x19


Qwiic_Relay relay(RELAY_ADDR);

////////////////

/////////////////crypto

#include <SparkFun_ATECCX08a_Arduino_Library.h> //Click here to get the library: http://librarymanager/All#SparkFun_ATECCX08a
#include <Wire.h>

ATECCX08A atecc;

uint8_t token[32]; // time to live token, created randomly each authentication event

uint8_t signature[64]; // incoming signature from Alice

int headerCount = 0; // used to count incoming "$", when we reach 3 we know it's a good fresh new message.

// Alice's public key.
// Note, this will be unique to each co-processor, so your will be different.
// copy/paste Alice's true unique public key from her terminal printout in Example6_Challenge_Alice.

uint8_t AlicesPublicKey[64] = {
  0x38, 0xD6, 0xE5, 0x49, 0xAC, 0x57, 0x2D, 0x1F, 0xD0, 0x58, 0x0A, 0xE8, 0x59, 0xB8, 0xF8, 0x20,
  0x1E, 0x0A, 0x7E, 0x8D, 0x5B, 0x7D, 0xD9, 0x8A, 0x26, 0xAF, 0x88, 0x73, 0x6D, 0x8C, 0xB7, 0x2D,
  0x8D, 0x3A, 0xB9, 0x5F, 0x60, 0x9D, 0x3F, 0x49, 0x72, 0xF1, 0x44, 0x74, 0x82, 0x3F, 0x7B, 0xCF,
  0x1F, 0x18, 0xD3, 0xA4, 0xBF, 0x62, 0x15, 0xCC, 0xAF, 0xAD, 0x7E, 0x03, 0xD8, 0xE9, 0x93, 0x7E
};

void setup()
{
  pinMode(LED, OUTPUT);
  pinMode(successLED, OUTPUT);
  pinMode(failLED, OUTPUT);
  pinMode(statLED, OUTPUT);

  SerialUSB.begin(115200);
  // It may be difficult to read serial messages on startup. The following
  // line will wait for serial to be ready before continuing. Comment out if not needed.
  //while (!SerialUSB);
  SerialUSB.println("RFM Server!");

  //Initialize the Radio.
  if (rf95.init() == false) {
    SerialUSB.println("Radio Init Failed - Freezing");
    while (1);
  }
  else {
    // An LED indicator to let us know radio initialization has completed.
    SerialUSB.println("Receiver up!");
    digitalWrite(LED, HIGH);
    delay(500);
    digitalWrite(LED, LOW);
    delay(500);
  }

  rf95.setFrequency(frequency);

  // The default transmitter power is 13dBm, using PA_BOOST.
  // If you are using RFM95/96/97/98 modules which uses the PA_BOOST transmitter pin, then
  // you can set transmitter powers from 5 to 23 dBm:
  // rf95.setTxPower(14, false);


  Wire.begin();

  if (atecc.begin() == true)
  {
    SerialUSB.println("Successful wakeUp(). I2C connections are good.");
  }
  else
  {
    SerialUSB.println("Device not found. Check wiring.");
    while (1); // stall out forever
  }

  if (!relay.begin())
  {
    Serial.println("Check connections to Qwiic Relay.");
    while (1); // stall out forever
  }
  else
  {
    Serial.println("Qwiic Relay is ready to go.");
  }

}

void loop()
{
  if (rf95.available()) {
    // Should be a message for us now

    uint8_t len = sizeof(buf);

    if (rf95.recv(buf, &len)) {
      digitalWrite(LED, HIGH); //Turn on status LED
      timeSinceLastPacket = millis(); //Timestamp this packet

      SerialUSB.print("Got message: ");
      printBuf64();
      //SerialUSB.print(" RSSI: ");
      //SerialUSB.print(rf95.lastRssi(), DEC);
      SerialUSB.println();

      // if message from Alice is "$$$", Send a random token for her to sign.
      if (buf[0] == '$' && buf[1] == '$' && buf[2] == '$')
      {
        SerialUSB.println("Received $$$. Creating a new random TTL-token now...");

        // update library instance public variable.
        atecc.updateRandom32Bytes();

        uint8_t toSend[32];
        // copy from library public variable into our local variable
        for (int i = 0 ; i < 32 ; i++)
        {
          token[i] = atecc.random32Bytes[i]; // store locally
        }

        rf95.send(token, sizeof(token));
        rf95.waitPacketSent();
        SerialUSB.println("Sent token");
        digitalWrite(LED, LOW); //Turn off status LED
      }
      else // this means Alice just sent us a signature
      {
        SerialUSB.println("Received signature. Verifying now...");
        for (int i = 0 ; i < 64 ; i++) signature[i] = buf[i]; // read in signature from buffer.
        printSignature();
        // Let's verirfy!
        if (atecc.verifySignature(token, signature, AlicesPublicKey))
        {
          SerialUSB.println("Success! Signature Verified.");
          // Let's turn on the relay...
          relay.turnRelayOn();
          delay(1000);
          // Let's turn that relay off...
          relay.turnRelayOff();
          blinkStatus(successLED);
        }
        else
        {
          SerialUSB.println("Verification failure.");
          blinkStatus(failLED);
        }
      }

    }
    else
      SerialUSB.println("Recieve failed");
  }
  //Turn off status LED if we haven't received a packet after 1s
  if (millis() - timeSinceLastPacket > 1000) {
    digitalWrite(LED, LOW); //Turn off status LED
    timeSinceLastPacket = millis(); //Don't write LED but every 1s
    clearBuf();
    // destory token, to require a new cycle if this doesn't complete within 1 second
    for (int i = 0 ; i < 32 ; i++)
    {
      token[i] = 0x00;
    }
  }
}


void printSignature()
{
  SerialUSB.println("uint8_t signature[64] = {");
  for (int i = 0; i < sizeof(signature) ; i++)
  {
    SerialUSB.print("0x");
    if ((signature[i] >> 4) == 0) SerialUSB.print("0"); // print preceeding high nibble if it's zero
    SerialUSB.print(signature[i], HEX);
    if (i != 63) SerialUSB.print(", ");
    if ((63 - i) % 16 == 0) SerialUSB.println();
  }
  SerialUSB.println("};");
  SerialUSB.println();
}

void printBuf64()
{
  SerialUSB.println();
  SerialUSB.println("uint8_t buf[64] = {");
  for (int i = 0; i < 64 ; i++)
  {
    SerialUSB.print("0x");
    if ((buf[i] >> 4) == 0) SerialUSB.print("0"); // print preceeding high nibble if it's zero
    SerialUSB.print(buf[i], HEX);
    if (i != 63) SerialUSB.print(", ");
    if ((63 - i) % 16 == 0) SerialUSB.println();
  }
  SerialUSB.println("};");
  SerialUSB.println();
}

void clearBuf()
{
  for (int i = 0; i < 64 ; i++) buf[i] = 0x00;
}

void blinkStatus(int LED)
{
  digitalWrite(LED, HIGH);
  delay(2000);
  digitalWrite(LED, LOW);
  delay(500);
}