SAMD21 Mini/Dev Breakout Hookup Guide

≡ Pages
Contributors: jimblom

Hardware Setup

To power the SAMD21 Breakout board, just plug it into a USB port on your computer. The red power LED indicator should immediately turn on, followed shortly-thereafter by a blinking blue LED on pin 13.

SAMD21 boards plugged in

Soldering Tips

You can set the SAMD21 Boards up -- and start programming them -- without connecting anything besides a USB cable, but you're not going to get far without soldering something to them. That something can be headers (male, female, right-angle or more) or just plain-old wire.

Hook-Up Wire - Assortment (Solid Core, 22 AWG)

PRT-11367
$25.95

Straight Header - Male (PTH, 0.1in., 40-Pin)

PRT-00116
$1.95

Stackable Header - Female (PTH, 0.1in., 6-Pin)

PRT-09280
$0.80

Straight Header - Female (PTH, 0.1in., 40-Pin)

PRT-00115
$1.95

If you're using a Mini Breakout, a pair of 12-pin male headers work well to keep the board breadboard-friendly. A 2-pin female header can be soldered to the inner I2C pins -- though you may have to trim the bottom side of the shroud to avoid the ATSAMD21's pins.

SAMD21 Mini Board assembled

SAMD21 Mini Breakouts assembled with male headers and 6-pin stackable headers. Female headers have to be trimmed a bit to avoid components.

Two pairs of 6-pin stackable headers can also maintain breadboard-compatibility while allowing your to jumper straight out of the board. To use these headers, you'll have to shave a bit of the bottom edge of the shroud to avoid bumping up against the outer LEDs.

If you're using the Dev Breakout, you can keep it Arduino-shield-compatible by soldering a handful of female headers into the 6-, 8-, and 10-pin headers. Then solder some 3-pin male headers into the SPI port.

SAMD21 Dev Board assembled

Finish it off by adding a PTH Barrel Jack and a set of standoffs and 1/4" 4-40 screws.