RFM69HCW Hookup Guide

≡ Pages
Contributors: MikeGrusin

The Antenna

IMPORTANT: You MUST attach an antenna to the board. Aside from not working without an antenna, transmitters can be damaged if they transmit without an antenna present.

Creating an antenna is not as hard as it may sound. The simplest antenna is a wire cut to the proper length and soldered to the "A / ANT" pin. The length depends on the frequency of your board and is marked on the bottom of the board for your convenience:

RFM69 back

Frequency Length (inches) Length (mm)
915 MHz 3.07" (3 + 1/16") 78mm
434 MHz 6.47" (6 + 1/2") 164mm

FYI: This is called a quarter-wave antenna because the length is one-quarter of a full wavelength at the transmission frequency.

PROTIP: Cut the antenna wire slightly longer to give yourself room to strip one end and solder it to your board. You can always trim it to the proper length after you solder it down.

Antenna Placement

For antenna placement you have a few options:

Single Antenna

The simplest option is to solder a properly-sized antenna wire to the "A" / "ANT" header hole (the one with the circle around it), and stick it straight up. That's it!

alt text

PROTIP: If you can, keep all of the antennas in your network as vertical as possible. The radiation pattern from a vertical antenna is shaped like a donut laying on a table, with the strongest signal out to the sides and the weakest signal above and below (where the hole is). Keeping your antennas vertical will maximize the horizontal distance that your signal will reach.
IMPORTANT: Radio waves will pass through plastic, but will be blocked by metal. Your radio module and antenna will work within a plastic box, but not a metal one.

If you need the antenna to be shorter to fit within a plastic box, you can bend or coil the antenna (this will adversely affect the range and directionality), but don't change the length unless you know what you're doing.

If you're using a metal box, you should pass the antenna through a hole and extend it outside the box (see below). Also try to keep your radio module and antenna away from large metal objects, as the metal will disrupt the transmission.

You will get good results from this basic antenna, but if you want to maximize your range, consider the following options as well:

Add a Dipole

Antennas love to have a ground underneath them. The RFM69HCW board contains a ground, but, the larger the ground, the better. A dipole is an antenna that has an equal length of grounded wire extending below the board. This creates a virtual ground that will increase the gain of the antenna.

To make a dipole, cut a second wire the same length as your antenna, solder it to one of the "G" / "GND" header holes adjacent to the antenna, and point it in the opposite direction of the antenna (straight down instead of up).

alt text

Keep both wires straight, in free air, and away from large metal objects if possible.

Remote Mounting

You can mount the antenna a short distance away from the board by (ideally) using 50-ohm coaxial cable, or (less ideally) by running a ground wire next to it. At the point where your antenna begins, simply end the coaxial shield / ground wire, or connect it to your ground plane (see below) or dipole. (The unshielded portion of your antenna should be 1/4-wave long as discussed above).

alt text

alt text

Using a Ground Plane

Because antennas love to have a ground underneath them, the best antennas stick up above a well-grounded surface. If you're using a metal box,or mounting the antenna on a vehicle roof, you can extend the antenna through and above the metal surface, as long as the surface is grounded. (Ensure that the antenna conductor doesn't short out against the ground plane where it passes through it.) If you don't have a handy metal surface you can create workable ground planes with a grid of copper tape or foil, radial grounded wires, etc.

alt text

alt text

Connecting a Commercial Antenna

If you'd like to connect a commercially-available antenna, you can solder an SMA Connector to the RFM69HCW board. Position the connector over the three headers marked G / A / G, and solder on both sides to ensure a good connection.

IMPORTANT: Note that the above connector is SMA, not RP-SMA ("Reverse Polarity"). Ensure that your antenna has a true male SMA connector and was designed for the radio frequency of your RFM69HCW (915MHz or 430MHz).

Other Antenna Types

The quarter-wave antenna is simple and effective, but, if you need additional range, there are other antenna designs like the Yagi that are far more directional, which is useful if you can point your antennas towards each other.

We're not antenna experts, so this is where we'll leave you. But if you're interested in this topic, consider getting involved in amateur radio. It's a great way to learn about antenna design and many other things: www.arrl.org.