RFID Beginners Tutorial

≡ Pages
Contributors: Brandon J. Williams

Introduction

In this tutorial we'll show you how to make a remote "clock punch" that logs time, location, and identification.

RFID is as magic as waving a card in front of a little black box and doors open for all to pass. This technology is so versatile that it was projected in 2017 to support a $31.42 billion market by 2023. We’ve enjoyed RFID tech as much as the next and we want to share it with you. In this tutorial we’ll touch on some key topics of the technology. Then we’ll work on making a remote work clock punch that can log time, location, and identification. Who knows, maybe you’ll find your own magic in RFID as well.

Items we will be using in this tutorial.

What Is RFID?

In simple terms, RFID Technology is a method of wireless communication between two (or more) electrical components. There is a reader that can emit a signal and passively reads incoming signals. Tags are devices that contain identification or other information. They come in two types, passive or active. Active tags have their own power source to actively transmit their contained information. Passive tags are ‘powered’ through radiated signals from the reader to transmit unique information. Either way it boils down to two devices yelling at each other like two cranky people. This transmission is how we’ll pass this information to our microcontroller to log our "in’s and out’s".

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Suggested Reading

Before going further, brave adventurer, please feel free to brush up on other tutorials and content that will help you on your journey.

GPS Basics

The Global Positioning System (GPS) is an engineering marvel that we all have access to for a relatively low cost and no subscription fee. With the correct hardware and minimal effort, you can determine your position and time almost anywhere on the globe.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.

RFID Basics

Dive into the basics of Radio Frequency Identification (RFID) technology.

SparkFun Qwiic RFID-IDXXLA Hookup Guide

The Qwiic RFID ID-XXLA is an I2C solution that pairs with the ID-LA modules: ID-3LA, the ID-12LA, or the ID-20LA, and utilizes 125kHz RFID chips. Let's take a look at the hardware used for this tutorial.

SparkFun GPS Breakout (ZOE-M8Q and SAM-M8Q) Hookup Guide

The SparkFun ZOE-M8Q and SAM-M8Q are three similarly powerful GNSS boards, but with different project applications. We'll compare both GNSS receivers before getting each up and running.

Displaying Your Coordinates with a GPS Module

This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).

Hookup Guide for the SparkFun RedBoard Artemis Nano

Get started with the powerful RedBoard Artemis Nano

Qwiic Connect System
Qwiic Connect System

Hardware Overview

We'll be using the Artemis Nano to read the RFID tags and GPS modules. We will be using Arduino to program the Artemis nano. For more information about each component, click on the links to the product pages.

Artemis Nano

"With 1MB flash and 384k RAM you'll have plenty of room for your sketches. The Artemis module runs at 48MHz with a 96MHz turbo mode available and with Bluetooth to boot! The SparkFun Artemis Nano is an incredibly flexible device for a small footprint..."

Qwiic RFID Reader

"The SparkFun RFID Qwiic Kit is a simple, yet all-in-one I2C based RFID starting point for the ID-3LA, ID-12LA, and ID-20LA readers. Simply plug a reader into the headers and use a Qwiic cable to connect to any Qwiic enabled development board, then scan your 125kHz ID tag and the unique 32-bit ID will be shown on the screen."

SAM-M8Q - Chip Antenna

"The SparkFun SAM-M8Q GPS Breakout is a high quality, GPS board with equally impressive configuration options. The SAM-M8Q is a 72-channel GNSS receiver, meaning it can receive signals from the GPS, GLONASS, and Galileo constellations. This increases precision and decreases lock time and thanks to the onboard rechargable battery, you'll have backup power enabling the GPS to get a hot lock within seconds!"

Hardware Hookup

As far as the hardware is concerned, we’re going to lean hard on the Qwiic ecosystem. This ecosystem allows us to easily connect devices together without needing to solder. No mess, no fuss!

SparkFun Artemis Nano, Qwiic RFID Reader and Qwiic GPS connected together.

Software

Note: This code/library has been written and tested on Arduino IDE version 1.8.12 . Otherwise, make sure you are using the latest stable version of the Arduino IDE on your desktop.

If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Our final code will be a mash up of two basic examples for our components. We’ll take a quick look at each part of the examples that we’ll use and talk about the main points.

Qwiic RFID Reader

The Qwiic RFID library will give you the full functionality of the Qwiic RFID ID-XXLA without the hub bub of the I²C data transactions. Also included are examples codes to demonstrate the full functionality of the library. You can click the link below to download the file directly and install it manually, or navigate through the Arduino Library Manager by searching SparkFun Qwiic RFID. You can also go the GitHub page and get download it from there.

Qwiic RFID Reader connected to the SparkFun Artemis Nano

In the Read_Tag_Basics example, the reader logs all tags that are recognized in a memory buffer. We read the buffer and clear it for a new read. We see that functionality below:

language:c
serialInput = Serial.read(); 
if (serialInput == 49){   // "1" on your keyboard is 49 in ASCII
  tag = myRfid.getTag();
  Serial.print("Tag ID: ");
  Serial.print(tag);
  scanTime = myRfid.getPrecReqTime(); 
  // If this time is too precise try: 
  // long time = myRfid.getReqTime(); 
  Serial.print(" Scan Time: ");
  Serial.println(scanTime);
}

Serial.read(); reads the buffer into the micro-controller's memory and clears the reader's buffer for another swipe. The tag is printed in the serial output along with the scan time. What we need to take away from this is the Serial.read(); and myRfid.getTag();.

SAM-M8Q GPS Module

The SparkFun U-blox Arduino library can be downloaded with the Arduino library manager by searching 'SparkFun Ublox' or you can grab the zip here from the GitHub repository:

SAM-M8Q GPS connected to the SparkFun Artemis Nano

Using SparkFun’s u-blox Arduino Library and Example2_NMEAParsing.ino, we’ll get our GPS coordinates and time. If you look closely at the code below, you’ll notice that something is missing:

language:c
long latitude_mdeg = nmea.getLatitude();
long longitude_mdeg = nmea.getLongitude();

Serial.print("Latitude (deg): ");
Serial.println(latitude_mdeg / 1000000., 6);
Serial.print("Longitude (deg): ");
Serial.println(longitude_mdeg / 1000000., 6);

We’re missing functions to get time. However, if we look at the u-blox library header file we can see the following functions that we’ll add in to the final code similarly to how the latitude and longitude functions are called in the example:

language:c
uint16_t getYear(uint16_t maxWait = getPVTmaxWait);
uint8_t getMonth(uint16_t maxWait = getPVTmaxWait);
uint8_t getDay(uint16_t maxWait = getPVTmaxWait);
uint8_t getHour(uint16_t maxWait = getPVTmaxWait);
uint8_t getMinute(uint16_t maxWait = getPVTmaxWait);
uint8_t getSecond(uint16_t maxWait = getPVTmaxWait);

These functions will give us time. Now let's combine all our parts. The full code is below:

language:c
/******************************************************************************
Remote Work Punch Clock
brandon.williams@sparkfun.com
May 6, 2019

Description When a card is read then the GPS coordinates and time are read from
    the GPS module.

Development environment specifics:
Arduino IDE 1.8.12 (or most recent)

Board Definition Packages (or most recent):
  SparkFun Apollo3 Boards           1.1.1
  MicroNMEA                         2.0.1
  SparkFun_Qwiic_Rfid.h             1.1.6
  SparkFun_u-blox_GNSS_Arduino_Library    2.0.2
******************************************************************************/


#include <MicroNMEA.h>

#include <SparkFun_Qwiic_Rfid.h>

#include <SparkFun_u-blox_GNSS_Arduino_Library.h>//http://librarymanager/All#SparkFun_u-blox_GNSS


#define RFID_ADDR 0x7D // Default Qwiic RFID I2C address

// Variables and Constants
      /*GPS*/
SFE_UBLOX_GNSS myGNSS;
char nmeaBuffer[100];
MicroNMEA nmea(nmeaBuffer, sizeof(nmeaBuffer));
      /*RFID*/
Qwiic_Rfid myRFID(RFID_ADDR);
String tag;
float scanTime;
int serialInput;

void setup() {

  Wire.begin();
  //Disable Serial after confirming setup works
  Serial.begin(115200);

  /*Qwiic RFID begin*/
  if(myRFID.begin()== false){
    Serial.println("Could not communicate with Qwiic RFID!");
    while(1);
  }

}

void loop() {

  /*RFID loop code*/
  tag = myRFID.getTag();

  /* Empty string is returned if no tag is present,
   * wait till a valid ID string is returned.
   */
    if(myGNSS.begin() != false){
      if(tag.length() != 6){
        Serial.print("Tag ID: ");
        Serial.println(tag);

        /*GPS loop code*/
        myGNSS.checkUblox(); //See if new data is available. Process bytes as they come in.

        if(nmea.isValid() == true){
          if(nmea.getNumSatellites() != 0){
            long latitude_mdeg = nmea.getLatitude();
            long longitude_mdeg = nmea.getLongitude();
            uint16_t dateYear =  nmea.getYear();
            uint8_t dateMonth = nmea.getMonth();
            uint8_t dateDay = nmea.getDay();
            uint8_t dateHour = nmea.getHour();
            uint8_t dateMin = nmea.getMinute();
            uint8_t dateSec = nmea.getSecond();

            //Print Coordinates
            Serial.print("Latitude (deg): ");
            Serial.println(latitude_mdeg / 1000000., 6);
            Serial.print("Longitude (deg): ");
            Serial.println(longitude_mdeg / 1000000., 6);

            //Print Time
            Serial.print("Date and Time: ");
            Serial.print(dateMonth);
            Serial.print("-");
            Serial.print(dateDay);
            Serial.print("-");
            Serial.print(dateYear);
            Serial.print(" @ ");
            Serial.print(dateHour);
            Serial.print(":");
            Serial.print(dateMin);
            Serial.print(":");
            Serial.println(dateSec);
          }
        }
        else{
          Serial.print("No Fix - ");
          Serial.print("Num. satellites: ");
          Serial.println(nmea.getNumSatellites());
        }
      }
      delay(500);
    }
}

//This function gets called from the SparkFun Ublox Arduino Library
//As each NMEA character comes in you can specify what to do with it
//Useful for passing to other libraries like tinyGPS, MicroNMEA, or even
//a buffer, radio, etc.
void SFE_UBLOX_GNSS::processNMEA(char incoming)
{
  //Take the incoming char from the Ublox I2C port and pass it on to the MicroNMEA lib
  //for sentence cracking
  nmea.process(incoming);
}

When we swipe a card over the scanner then we should get something like below:

Serial Output RFID Tag Location

Troubleshooting

Resources and Going Further

This tutorial is just a first step into making a larger RFID project. Stay tuned for a more advanced tutorial to expand beyond just reading data in a serial monitor.

In the meantime, please feel free to visit more RFID tutorials and learn new skils:

SparkFun RFID Starter Kit Hookup Guide

Learn the basics of how to get started with the SparkFun RFID Starter Kit.

SparkFun Qwiic RFID-IDXXLA Hookup Guide

The Qwiic RFID ID-XXLA is an I2C solution that pairs with the ID-LA modules: ID-3LA, the ID-12LA, or the ID-20LA, and utilizes 125kHz RFID chips. Let's take a look at the hardware used for this tutorial.

Qwiic Dynamic NFC/RFID Tag Hookup Guide

Add a configurable NFC/RFID tag to your Qwiic ecosystem by following this guide.

How To Take Multiple RFID Readings Simultaneously

Let's take an in-depth look at how to take multiple RFID readings at once with a SparkFun Simultaneous RFID Reader.

 

FPGA chip