RETIRED - Pi Wedge Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

View the updated tutorial: RETIRED - Pi Wedge B+ Hookup Guide

≡ Pages
Contributors: Byron J.

Pin Mapping

Revisions

The pins on the Raspberry Pi changed between Revision 1 and Revision 2 - a few signals were reassigned. The physical connection is the same, but you'll need to know which version of Pi you're using to address the pins correctly.

The Wedge is labeled with the Revision 2 labels. You'll need to translate a few things if you're using a Revision 1 Pi. In short - to use the Wedge with a Revision 1 Raspberry Pi, do the following.

  • Be sure to use /dev/I2C0 instead of /dev/I2C1.
  • Use GPIO 21 instead of GPIO 27.

Alternately, use a software library such as Wiring Pi that can identify the revision and abstract the pin numbers. We'll cover WiringPi in more detail in the software section.

Signal Location

The Pi Wedge reorganizes the I/O pins on the Pi, putting similar functions on adjacent pins. The SPI, I2C and UART signals are all grouped near each other.

Pin function diagram

Functional Groupings

The pins are labeled, though the labels are short to fit the space available on the PCB. The UART, SPI and I2C pins are marked with their communication bus functions, but they can also available as GPIO pins when initialized in that mode.

The following table denotes the assignment of signals on the Pi Wedge, including the peripheral and alternate GPIO assignments where appropriate.

Function GPIO# Function GPIO#
Ground R0: SCL0
R1: SCL1
R0: GPIO1
R1: GPIO3
SPI0 Chip Enable 1 GPIO 7 R0: SDA0
R1: SDA1
R0: GPIO0
R1: GPIO2
SPI0 Chip Enable 0 GPIO 8 R1: GPIO 21
R2: GPIO 27
SPI0 MOSI GPIO 10 GPIO 25
SPI0 MISO GPIO 9 GPIO 24
SPI0 Shift Clock GPIO 11 GPIO 23
UART Rx GPIO 15 GPIO 22
UART Tx GPIO 14 GPIO 18
GPIO 4 GPIO 17
5V 5V
3.3V 3.3V
Ground Ground