RedBoard Edge Hookup Guide

≡ Pages
Contributors: Englandsaurus

Download/Install Arduino

Before you plug the RedBoard Edge into your computer, you'll need to install Arduino first.

Installing Arduino

To begin, head over to Arduino's download page and grab the most recent, stable release of Arduino. Make sure you grab the version that matches your operating system.

The installation procedure is fairly straightforward, but it varies by OS. Here are some tips to help you along. We've also written a separate Installing Arduino tutorial if you get really stuck.

Installing Arduino IDE

March 26, 2013
A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Windows Install Tips

The Windows version of Arduino is offered in two options: an installer or a zip file. The installer is the easier of the two options, just download that, and run the executable file to begin installation. If you're prompted to install a driver during installation, select "Don't Install" (the RedBoard Edge doesn't use the same drivers). Don't forget which directory it installs to (defaults to "Program Files/Arduino").

Windows Installer

Windows install steps. Click the image to get a bigger view.

If, instead, you choose to download the zip file version of Arduino, you'll need to extract the files yourself. Don't forget which folder you extract the files into! We'll need to reference that directory when we install drivers.

Mac Install Tips

The Mac download of Arduino is only offered in a zip file version. After the download is finished, simply double-click the .zip file to unzip it.

Mac Install Screenshot

Following that, you'll need to copy the Arduino application into your applications folder to complete installation.

Linux Install Tips

As you Linux users are no doubt aware, there are many flavors of Linux out there, each with unique installation routines. Check out the Linux section of the Installing Arduino tutorial for some helpful links for an assortment of Linux distributions.

For Ubuntu and Debian users, installing Arduino should be as easy as running a little "apt-get" magic, with a command like:

language:bash
sudo apt-get update && sudo apt-get install arduino arduino-core  

And other Linux distros aren't too dissimilar from that.


With Arduino downloaded and installed, the next step is to plug the RedBoard Edge in and install some drivers! Pretty soon you'll be blinking LEDs, reading buttons, and doing some physical computing!