Qwiic Ultrasonic Distance Sensor (HC-SR04) Hookup Guide

≡ Pages
Contributors: Ell C

Software Setup and Programming

Note: Make sure you are using the latest stable version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-on, please review the following tutorials.

Our friends over at Zio have provided an example to get you started with this Ultrasonic Distance Sensor. In order to do so, you'll need to install a few libraries first.

To display the sensor readings on the connected Qwiic OLED, we will use three Adafruit libraries:

Adafruit BusIO Library

You can install this library to automatically in the Arduino IDE's Library Manager by searching for "Adafruit BusIO". Or you can manually download it from the GitHub repository.

Adafruit GFX Library

You can install this library to automatically in the Arduino IDE's Library Manager by searching for "Adafruit GFX". Or you can manually download it from the GitHub repository.

Adafruit SSD1306 Library

You can install this library to automatically in the Arduino IDE's Library Manager by searching for "Adafruit SSD1306 Library". Or you can manually download it from the GitHub repository.


Example 1

This example lives in the GitHub Repo in the Arduino folder. Feel free to download the code, alternatively you can copy the code below into a blank Arduino sketch. Select your board (for this example we'd select "SparkFun RedBoard") and the port your board has enumerated on. Go ahead and upload your code.

language:c
#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>
#define SLAVE_BROADCAST_ADDR 0x00  //default address
#define SLAVE_ADDR 0x00       //SLAVE_ADDR 0xA0-0xAF
uint8_t distance_H = 0;
uint8_t distance_L = 0;
uint16_t distance = 0;

#define SCREEN_WIDTH 128 // OLED display width, in pixels
#define SCREEN_HEIGHT 32 // OLED display height, in pixels

// Declaration for an SSD1306 display connected to I2C (SDA, SCL pins)
#define OLED_RESET     4 // Reset pin # (or -1 if sharing Arduino reset pin)
Adafruit_SSD1306 display(SCREEN_WIDTH, SCREEN_HEIGHT, &Wire, OLED_RESET);


void setup() {
  Wire.begin(); // join i2c bus (address optional for master)
  Serial.begin(9600);  // start serial for output
  display.begin(SSD1306_SWITCHCAPVCC, 0x3C);  // initialize with the I2C addr 0x3C (for the 128x32)
  Serial.println("IIC testing......");
  display.clearDisplay();
  //  Wire.beginTransmission(SLAVE_BROADCAST_ADDR); // transmit to device SLAVE_BROADCAST_ADDR
  //  Wire.write(SLAVE_ADDR);              // Change the SLAVE_ADDR
  //  Wire.endTransmission();    // stop transmitting
}



void loop() {
  Wire.beginTransmission(SLAVE_ADDR); // transmit to device #8
  Wire.write(1);              // measure command: 0x01
  Wire.endTransmission();    // stop transmitting

  Wire.requestFrom(SLAVE_ADDR, 2);    // request 6 bytes from slave device #8
  while (Wire.available()) { // slave may send less than requested
    distance_H = Wire.read(); // receive a byte as character
    distance_L = Wire.read();
    distance = (uint16_t)distance_H << 8;
    distance = distance | distance_L;
    Serial.print(distance);         // print the character
    Serial.println("mm");
    display.setTextSize(2);
    display.setTextColor(WHITE);
    display.setCursor(10, 0);
    display.clearDisplay();
    display.print(distance);
    display.print("mm");
    display.display();
    delay(1);

    delay(100);
  }
}

Try moving an object (like your hand or a dinosaur) closer to the sensor - notice the output of the OLED shows you how close the object is! Grr. Rawr!

Oh no! A dinosaur is approaching distance sensor and now it's only 61mm away!

Curse your sudden but inevitable betrayal!