Comments: Qwiic ToF Imager - VL53L5CX Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #1686721 / about 2 years ago / 1

    if I remove the while() loop, it seems to process correctly.. like the status is temporary, read once..

  • Member #1686721 / about 2 years ago / 1

    I am using this on an ESP32 WROOM processor, and getting inconsistant results on
    myImager.isDataReady()

    my code .... startRanging(); delay(5); while(!myImager.isDataReady()){ delay(5); } if (myImager.isDataReady() == true) { if (myImager.getRangingData(&measurementData)) // Read distance data into array { // } }

    i get thru the while loop,, which says data IS ready but the if (myImager.isDataReady() == true) says NOT ready, ever..

    if I comment this out, the readdata works, and presents differing results as an object moves thru the sensor space. as expected the distances reported by the cells are accurate/ (only testing 600-4000mm)

    in looking at the library code, the isReady checks the rc from the ST library function, and if 0 (ok) it then returns the result of if (result == 0) return dataReady != 0;

    I am getting 0 (not true),. so that means dataReady is zero.. I think dataReady is the value described in doc UM2884, page 14 rc 5 is good.. the rest (6 & 9) are suspect at best

  • Member #220843 / about 4 years ago * / 1

    Hey, this is not perfect, but there's a fantastic micropython / circuitpython module by Mark Grosen at https://github.com/mp-extras/vl53l5cx

    I had problems using the mini breakout due to having no low-power pin on the breakout, so I forked and fixed the module.

    https://github.com/tyeth/vl53l5cx/blob/main/examples/sparkfun_micro_vl53l5cx.py

    I added an example file that outputs comma-separated values (suitable for the Sparkfun Processing.org Visualisation like arduino example 4), designed for the Sparkfun RP2040 connected to Sparkfun Qwiic ToF Mini VL53L5CX breakout (should work on most boards).


If you've found an issue with this tutorial content, please send us your feedback!