Qwiic Micro OLED Hookup Guide

≡ Pages
Contributors: Englandsaurus

Hardware Overview

Listed below are some of the operating ranges and characteristics of the Qwiic Micro OLED.

Characteristic Range
Voltage 3.3V
Temperature -40°C to 85°C
I2C Address 0X3D (Default) or 0X3C (Closed Jumper)

Pins

Power and I2C pins are broken out to the 1x4 PTH pins as well as the two horizontal Qwiic connectors.

PinDescriptionDirection
GNDGroundIn
3.3VPowerIn
SDADataIn
SCLClockIn

Jumpers

There are several jumpers on board that can be changed to facilitate several different functions. The first of which is the I2C pull-up jumper to disable the 2.2kΩ pull up resistors on the I2C data and clock lines, highlighted below. If multiple boards are connected to the I2C bus, the equivalent resistance goes down, increasing your pull up strength. If multiple boards are connected on the same bus, make sure only one board has the pull-up resistors connected.

I2C Pull-Up Jumper

The ADDR jumper (highlighted below) can be used to change the I2C address of the board. The default jumper is open by default, pulling the address pin high and giving us an I2C address of 0X3D. Closing this jumper will ground the address pin, giving us an I2C address of 0X3C.

Address Jumper

Board Dimensions

The overall board size is 1.08" x 1.17". There is a v-score for users that want to remove the mounting holes.

Board Dimensions