Photon IMU Shield Hookup Guide

≡ Pages
Contributors: b_e_n

IMU Shield Overview

Pin Descriptions

Since the shield does all of the work for you, there's no need to actually wire these connections - but in case you're looking at datasheets, or code examples, this table will give you a clue as to what the shield is doing. As always, you can check the schematic for more info.

alt text

IMU Shield Pin Photon Pin Function
GND GND Ground
VDD 3.3V Regulated 3.3V in
SCL D1 SCL Serial clock
SDA D0 Serial Data in


We also broke out a few pins at the top of the board that some of you may wish to make use of. From left to right in the picture above, they are:

IMU Shield Pin Function
DEN AG Data Enable Accel/Gyro
INT2 AG Programmable Interrupt Accel/Gyro
INT1 AG Programmable Interrupt Accel/Gyro
INT M Programmable Interrupt Magnetometer
DRDY M Magnetic sensor data ready


Setting the Jumpers

With the board flipped over, you'll notice there are six jumpers. The majority of these jumpers are used to switch between SPI and I2C mode. As the board ships, these jumpers are set to configure the IMU in I2C mode.

alt text

The SDO M-MISO and SDO A/G-MISO jumpers can be used to set the I2C addresses (In I2C mode) or, if open, can be used either to set I2C address or for SPI control. The default out of the box has both jumpers pulled high for I2C mode.

I2C Address Table

SDOM /AG AG Addr. M Addr.
0 0x6A 0x1C
1 0x6B 0x1E


The CS A/G-SS2 and CS M-SS are the chip select jumpers for the accelerometer/gyro and the magnetometer, respectively. The board ships with them both pulled high to enable I2C mode. Close the jumpers and cut the former traces to enable SPI mode.

The same story holds true for the SDA-MOSI and SCL-SCK jumpers. They are pulled high to enable I2C communication. Close the jumpers in the other direction and cut the former traces to enable SPI mode.