My Drunk Kitchen Apron

≡ Pages
Contributors: Dia

Special Sauce

You've got a beautiful apron and an awesome circuit, but the project lacks Hart, no? Here are four sets of audio clips you can choose from to finish up! Choose any 5 sounds clips from these downloads to associate with your 5 buttons!

Set 1: Food Related Quotes from MDK Episodes

  • Pin 1 (Grilled Cheese)
  • Pin 2 (Corndog)
  • Pin 3 (No Baking)
  • Pin 4 (Nachos)
  • Pin 5 (Taco)

Download the entire set here.

Set 2: Helpful Kitchen Advice from a Master

  • "I don't have any cheese!"
  • "I'm not afraid of anything!"
  • "You'll never know until you try!"
  • "Learn another language!"
  • "Always clean as you go!"

Download the entire set here.

Set 3: Custom Quotes Just for Aprons!

  • "Grilled Please!"
  • "Corn dogs are Delicious"
  • "No baking, because why bake when you can take a nap."
  • "Tacos are the most versitile fruit."
  • "Mmmmmmm."

Download the entire set here.

Set 4: One Liners

  • "Grilled Cheese"
  • "Corn Dog"
  • "Nachos"
  • "Taco"
  • No Baking"

Download the entire set here.


Uploading your chosen tracks to the MP3 trigger is a cinch! You'll need to pop your flash memory card into an SD card reader, and plug it into your computer.

When you unzip the sound files, you might notice that each file has a name that starts with a number between one and five. We've named the files to correspond with the pin that has the matching food in our diagram. If you moved the foods around and connected them to other pins, or if you cherry picked sound files and don't have one of each number, you'll need to change the names. The file you want to play when you press the button attached to pin one should start with the digit 1, pin two should start with 2, etc.

Once you've got one track with each number, save those to your memory card. Take it out of your card reader and pop it into the SD card slot on your MP3 trigger. It's that easy! Power it up, and try pressing the buttons to hear your sounds!