MP3 Player Shield Music Box

≡ Pages
Contributors: HelloTechie

Example Code

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Before uploading code, make sure to install the SFEMP3 library.

When you are ready, copy the following code and upload it to your Arduino!

language:c
//SFEMP3Library author Bill Porter
//SFEMP3Library author Michael P. Flaga
/* MP3 Player Shield Music Box Code Example:
  SparkFun Electronics, Pamela, 1/24/2013
  Beerware License

  Hardware Connections:
  -LED = D3 on MP3 Player Shield;
  -Motor = D5 on MP3 Player Shield;
  -Reed Switch = D4 on MP3 Player Shield;
  -Mono Audio Amp Breakout Board Shutdown Pin = D10 on MP3 Player Shield;
  You will need to solder header pins to the MP3 Player Shield.
  Put the shield on top of an Arduino Uno.

  Usage:
  When the door opens, the motor will spin and a sound file will play.
  The sound file will loop.
  Then when the door closes the motor stops spinning and a new track plays one time. */

#include <SPI.h>

//Add the SdFat Libraries
#include <SdFat.h>
#include <SdFatUtil.h>
//and the MP3 Shield Library
#include <SFEMP3Shield.h>

SFEMP3Shield MP3player;

int led = 3;
int motor = 5;
int reedSwitch = 4;
int speaker = 10;

int fadeAmount = 5;
int brightness = 0;
boolean active = false;


void setup() {
  pinMode(motor, OUTPUT); //Motor
  pinMode(led, OUTPUT); // LED
  pinMode(reedSwitch, INPUT); //Reed Switch
  pinMode(speaker, OUTPUT); //Speaker Enable

  analogWrite(led, 0); //LED off
  digitalWrite(reedSwitch, HIGH); //turn on internal pullups for reed input
  digitalWrite(motor, LOW); //Motor off

  MP3player.begin();
  MP3player.SetVolume(0x00, 0x00); //set volume
}

void loop() {

  if (digitalRead(reedSwitch) == HIGH && !active)//when door opens
  {
    active = true;
    analogWrite(led, 80);
    digitalWrite(speaker, HIGH);
    digitalWrite(motor, HIGH);
    MP3player.stopTrack();
    MP3player.playTrack(3);
  }
  else if (digitalRead(reedSwitch) == LOW && active)//when door closing
  {
    active = false;
    MP3player.stopTrack();
    MP3player.playTrack(2);
    digitalWrite(motor, LOW);
    analogWrite(led, 255);
  }
  else if (digitalRead(reedSwitch) == LOW) //while door is closed
  {
    analogWrite(led, 0);
    digitalWrite(motor, LOW);
  }
  else
  {
    MP3player.playTrack(1);
    analogWrite(led, brightness);
    if (brightness == 0 || brightness == 255) {
      fadeAmount = -fadeAmount;
    }
    brightness += fadeAmount;
  }

  delay(100);
}