microSD Sniffer Hookup Guide

≡ Pages
Contributors: Toni_K

Hardware Overview

Hardware wise, the microSD Sniffer is pretty simple and straight-forward! There's only 3 main parts you need to be aware of.

Front of Sniffer

Front view of the microSD Sniffer.

1. Headers

The pins of the SD card are broken out for a standard 0.1-inch row of header holes. This allows you to solder headers onto the board and connect into a breadboard for prototyping. Alternatively, you can also just connect IC hooks on these holes and use a logic analyzer or oscilloscope to monitor the traffic across the SPI bus.

2. microSD Socket

This is your standard microSD socket. It fits microSD cards. Hurray simplicity!

3. microSD Insert

Back of Sniffer

Back view of the microSD Sniffer.

These are the actual connection pins for the microSD Sniffer. You will plug these into your circuit in place of where you would normally plug in a microSD card. Notice how they look exactly like the bottom of your microSD card?