MicroMod STM32WB5MMG Hookup Guide

≡ Pages
Contributors: El Duderino

Hardware Assembly

If you have not already, make sure to check out the Getting Started with MicroMod: Hardware Hookup for information on properly inserting your Processor into your Carrier Board.

Getting Started with MicroMod

October 21, 2020
Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Start by inserting the MicroMod STM32WB Processor into your Main or Carrier Board at roughly a 45° angle similar to the image below:

Processor inserted into the MicroMod Main Board.

Next, secure the Processor in place using the set screw:

Processor secured to the MicroMod Main Board.

Connecting Everything Up

With your Processor inserted and secured it's time to connect your carrier board to your computer using the USB-C connector on the Carrier. Depending on which carrier you choose and which drivers you already have installed, you may need to install drivers.

alt text

Note: If you've never connected a CH340 device to your computer before, you may need to install drivers for the USB-to-serial converter. Check out our section on "How to Install CH340 Drivers" for help with the installation.

How to Install CH340 Drivers

August 6, 2019
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.