MicroMod Data Logging Carrier Board Hookup Guide
Contributors:
El Duderino,
Nate
Resources and Going Further
Hopefully this guide has got you all set to get started with your own MicroMod logging project using the SparkFun MicroMod Data Logging Carrier Board. For more information about the Carrier Board, check out the resources below:
For more information on the MicroMod ecosystem, check out these resources:
Not sure where to start with your own data logging project? The tutorials below may give you some ideas to get the creative juices flowing:
MicroSD Breakout With Level Shifter Hookup Guide
How to use the level translating µSD device.
Qwiic OpenLog Hookup Guide
The updated Qwiic version of the OpenLog Hookup Guide
OpenLog Artemis Hookup Guide
How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.
MicroMod Main Board Hookup Guide V2
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single V2.1 and Main Board - Double and V2.2.