LS20031 5Hz (66 Channel) GPS Receiver Hookup Guide

≡ Pages
Contributors: bitsmashed, followr, bboyho

Software Library Installation

Note: The examples assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Mikal Hart has written an excellent library to parse the GPS data. Click on the button below to download the TinyGPSPlus library.

You will need to install the library via the ZIP folder. Open Arduino, navigate to Sketch > Include Library > Add .ZIP Library, and select the ZIP folder you just downloaded.