Loading Debian (Ubilinux) on the Edison

≡ Pages
Contributors: Shawn Hymel

Log Into Ubilinux

Once you have flashed your Edison, you can log in over a serial connection.

IMPORTANT: If you are using the Intel Arduino or Mini-Breakout board, plug in the other USB cable at this time (you should have 2 USB cables running from your Edison to your computer). If you are using one of the SparkFun Edison Blocks with a "Console" port, you can use that port to power the Edison and receive a serial console.

Edison with Intel Arduino breakout board

You will need to use both USB ports on the Arduino Breakout board

Edison with SparkFun Base Block

You only need to use the USB port labeled "Console" on the Base Block

Windows

Download a serial terminal, such as PuTTY.

You will also likely need to download and install the Virtual COM Port Drivers from FTDI (download the "setup executable" version).

Open the Device Manager. Expand "Ports (COM & LPT)" and you should see a "USB Serial Port." Make a note of the COM number.

Finding the COM port number on Windows

Run PuTTY, select the "Serial" option, change the COM port number under "Serial line," and set the "Speed" to 115200.

Using PuTTY

Click "Open." You will see a blank terminal. Hit 'enter' and you will be prompted with a login screen.

Logging into Ubilinux using Windows

Enter the default login credentials:

ubilinux login: edison
Password: edison

And that's it! You are now logged into Ubilinux running on your Edison.

Mac OSX

Before you plug in your Edison, you need to find the location of the USB serial device. Open a terminal and enter:

ls /dev/tty.usb*

Make a note of which devices appear. Plug in your Edison (both cables for Intel breakout boards or the "Console" port for the SparkFun Blocks) and enter the command again:

ls /dev/tty.usb*

An extra file should appear. Remember the file name and use the screen command to connect:

screen /dev/tty.usbserial-XXXXXXXX 115200

Where -XXXXXXXX is the string of numbers and letters of the USB serial device. For example:

Using screen on OS X

Press 'enter' to see the login screen.

Logging in to Ubilinux on OS X

Enter the default login credentials:

ubilinux login: edison
Password: edison

You should now be logged into Ubilinux.

Linux

Open a terminal and connect using the screen command:

sudo screen /dev/ttyUSB0 115200

Note that your USB serial device may not be exactly ttyUSB0. If you have other USB serial devices plugged in, it could be ttyUSB1, ttyUSB2, and so on.

Press 'enter' to see the login screen.

Logging into Ubilinix using Linux

Enter the default login credentials:

ubilinux login: edison
Password: edison

You should now be logged into Ubilinux.