LilyPad Development Board Hookup Guide

≡ Pages
Contributors: jimblom, Gella

Uploading Code

You will need to perform the below three steps every time you want to program the board. These three steps are:

1. Connect the LilyPad Development Board to your computer using the FTDI board and a USB cable.
2. Select "LilyPad Arduino" from Arduino's "Board" menu.
3. Select "ATmega328" from Arduino's "Processor" menu.
4. Select the serial port the LilyPad is connected to from Arduino's "Port" menu.

Let's go over the three steps in detail:

1. Connect the LilyPad Development Board to Your Computer

Place the LilyPad Development Board on a clean, non-metal work surface. Connect the LilyPad FTDI Board to the headers on the LilyPad Arduino Simple at the center of the Development Board.

Attach FTDI to LilyPad Development Board

Connect the other side of the FTDI board to a mini-B USB cable.The cable can only be inserted one way, and should snap in securely.

Attach USB Cable to LilyPad Development Board

Then connect the other end of the USB cable to a USB port on your computer.

Connect LilyPad Development Board to Computer

Slide the switch on the LilyPad Arduino to the ON position. You will not be able to upload code to the board if it is set to the OFF position.

Turn LilyPad Development Board's Switch to ON Position

2. Select LilyPad Arduino from the Board Menu

To program the LilyPad Arduino Simple at the center of the LilyPad Development Board, open the Tools > Board list and select LilyPad Arduino. A dot (Windows) or check mark (Mac) will show next to the board in the menu when it is selected, and it will show next to Board in the Tools menu.

Select LilyPad Development Board in Arduino IDE

3. Select ATmega328 from the Processor Menu

After selecting the LilyPad Arduino, there will be two options available in the next menu down labeled Processor. Select ATmega328 for your LilyPad Arduino.

Select ATmega328 for LilyPad Development Board in Arduino IDE

4. Select Port from the Port Menu

Arduino needs to know which port your LilyPad Arduino is attached to so it can program it. Whenever you plug a USB device into your computer, your computer will assign it a port number. Go to the Tools > Port menu, and select the port that has the LilyPad Arduino attached to it.

On Windows ports are listed as COM##; on a Mac or Linux machine they will be "/dev/cu.usbmodem####". Your screen may look different than the image below, depending on what operating system you are using.

Select LilyPad Development Board's COM Port

Troubleshooting: If you don't see a port in the menu, ensure that the board is powered up (switch in the ON position), and that the USB cable is securely connected to both the board and your computer and that you have installed the FTDI drivers. Some USB cables are only meant for charging and don't pass data - they'll power the board, but it won't show up in the port menu. If needed, try a different cable.

Upload Blink

In the world of embedded electronics, every good development platform has to have an LED, and the first test program to be run on any development platform is almost always the blinking of an LED. So let's blink that little LED on the LilyPad Simple Arduino board.

To review, once you've:

  1. Connected the LilyPad Development Board to your computer using the FTDI and USB cable.
  2. Selected the board type ("LilyPad Arduino" as the board and ATmega328 as the processor).
  3. Selected the COM port from the "Port" menu.

You are ready to upload code! Let's upload some code to try it out.

Load the "Blink" example from the menu File > Examples > 01.Basics > Blink, and click the "Upload" button (the large round button with the right arrow in it). This is a very simple example program; it just blinks a LED on and off once per second.

Blink Example

Arduino will compile the code, then send it to the LilyPad Arduino Simple via the USB cable. While the code is uploading, the built-in LED will blink to signal the code is transferring. When the code finally runs, the LED at the center of the board will slowly blink green. Success!

If this all works, congratulations! You're all set up and ready to prototype with the LilyPad Development Board.

Default Example Code

If you are interested in re-uploading the default example code that you explored earlier, it is available in the product GitHub repository and in the download button shown below.

Beyond the Blinking

Well, we've just opened an enormous can of worms, and you've taken your first step into the life-consuming world of Arduino. From here, you may want to explore some of Arduino's other example sketches. There's one for the button (File > Examples > 2.Digital > Button), or you could fade those RGB LEDs (File > Examples > 1.Basics > Fade), or you could play a song on the buzzer (File > Examples > 2.Digital > toneMelody), or maybe try adapting the AnalogInOutSerial sketch (File > Examples > 3.Analog > AnalogInOutSerial) to the temperature and light sensors. Just make sure you change the pins to their proper mapping on the LilyPad Development Board!

Uploading to the LilyPad Development Board

You can also check out the LilyPad Development Board Activity Guide:

LilyPad Development Board Activity Guide

December 7, 2017
Learn how to program in Arduino with the LilyPad Development Board. This guide includes 11 example activities that use the pre-wired LilyPad boards on the LilyPad Development Board.