Lessons in Algorithms

≡ Pages
Contributors: Nate, barryjh

Where to Start

In full-fledged software projects, from an Engineer's perspective, you have four major phases:

  • Requirements
  • Design
  • Implementation
  • Test

Let’s face it; the design and coding is what everyone sees as interesting, where their creative juices can flow and the majority of the fun can be had. Naturally, there is the tendency to fixate on a certain aspect of the problem being solved and jump right in designing and coding. However, I will argue that the first and last phase can be the most important in any successful project, be it large or small. If you doubt that, consider this: my solution to the speed bag problem was designed wickedly fast, and I didn’t have a bag to test it on. But, with the right fixes applied in the end, the functionality was tested to verify that it produced the correct results. Conversely, a beautiful design and elegant implementation that doesn’t produce the required functionality will surely be considered a failure.

I didn’t mention prototype as a phase, because depending on the project it can happen in different phases or multiple phases. For instance, if the problem isn’t fully understood, a prototype can help figure out the requirements, or it can provide a proof of concept, or it can verify the use of a new technology. While important, prototyping is really an activity in one or more phases.

Getting back to the Speed Bag Challenge, in this particular case, even though it is a very small project, I suggest that you spend a little time in each of the four areas, or you will have a high probability of missing something important. To get a full understanding of what’s required, let's survey everything we had available as inputs. The web post for the challenge listed five explicit requirements, which you can find here. Next, there was a link to Nate’s Github repository that had information on the recorded data format and a very brief explanation of how the speed bag device would work.

In this case, I would categorize what Nate did with the first speed bag counter implementation as a prototype to help reveal additional requirements. From Nate’s write-up on how he built the system, we know it used an accelerometer attached to the base of a speed bag and that the vibration data samples about every 2ms are to be used to count punches. We also now know that applying a polynomial smoothing function and looking for peaks above a threshold doesn't accurately detect punches.

While trying not to be too formal for a small project, I kept these objectives (requirements) in mind while working the problem:

  • The algorithm shall be able to produce the correct number of hits from the recorded data sets
  • The solution shall be able to run on 8-bit and 32-bit micros
  • Produce documentation and help others learn from the solution put forth
  • Put code and documents in a public repository or website
  • Disclose the punch count and the solution produced for the Mystery data sets
  • Accelerometer attached to top of speed bag base, orientation unknown except +Z is up -Z is down
  • Complex data patterns will need more than polynomial filtering; you need to adjust to incoming data amplitude variations---as Nate suspects, resonance is the likely culprit
  • You have 15 days to complete (Yikes!)