Heating Pad Hand Warmer Blanket

≡ Pages
Contributors: HelloTechie

Example Code

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.
language:c
  /*

 Heating Pad Hand Warmer Blanket Code Example
  SparkFun Electronics, Pamela, 1/24/2013
  Beerware License

  Hardware Connections:
  -led1 = D9;
  -led2 = D10;
  -led3 = D11;
  -button = D2;
  -Mofset = D3;

  Usage: 
  Hit the switch to power, hit the button to adjust how warm the heating elements get, and three LEDs will indicate low, medium, and high levels. 
 */

int btnPin = 2;
boolean btnPressed = false;
int fetPin = 3;
int led1 = 9;
int led2 = 10;
int led3 = 11;
int mode;

void setup() {                
  // initialize the digital pin as an output.
  pinMode(btnPin, INPUT_PULLUP);  //set internal pull-up resistor for button
  pinMode(fetPin, OUTPUT);  
  pinMode(led1, OUTPUT);  
  pinMode(led2, OUTPUT);  
  pinMode(led3, OUTPUT);  
}

// the loop routine runs over and over again forever:
void loop() {
  //Increment mode on depress, unless mode = 3, then reset to 0
  if (btnPressed && digitalRead(btnPin) == LOW)
    mode = mode == 3 ? 0 : mode + 1;
  //Assign button state
  btnPressed = digitalRead(btnPin);
  switch (mode)
  {
    case 0:
      analogWrite(fetPin, 0); //off
      digitalWrite(led1, LOW);
      digitalWrite(led2, LOW);
      digitalWrite(led3, LOW);
      break;
    case 1:
      analogWrite(fetPin, 85); //33% duty cycle
      digitalWrite(led1, HIGH);
      digitalWrite(led2, LOW);
      digitalWrite(led3, LOW);
      break;
    case 2:
      analogWrite(fetPin, 170); //66% duty cycle
      digitalWrite(led1, HIGH);
      digitalWrite(led2, HIGH);
      digitalWrite(led3, LOW);
      break;
    case 3:
      analogWrite(fetPin, 255); //100% duty cycle
      digitalWrite(led1, HIGH);
      digitalWrite(led2, HIGH);
      digitalWrite(led3, HIGH);
      break;
  }
}

There you go! As with any DIY project, you should always customize and tweak what you want for maximum awesomeness.