Hackers in Residence - Cosmic Ray Detector

≡ Pages
Contributors: pmm223

Catching Some Rays

This project seeks to create an inexpensive cosmic ray detector capable of sensing rays greater than 1 GeV in energy. These can be used either as part of a timing synchronization solution, or as part of a large, distributed cosmic ray telescope.

The RayCatcher

The RayCatcher

WARNING!

This project deals with high voltage. Make certain to use appropriate precautions. Do not cut any wires while all batteries are connected; remove and replace batteries while wearing nitrile gloves if using standard battery clips. Drawer-type battery holders, such as the ones used in this project, do not necessitate the use of gloves.

Required Materials


Along with the parts listed above, you will also need a neon bulb.

Note that there are two options for battery holders. The less expensive one certainly works, but the more expensive one is safer, as it allows separation of the battery mechanically with no shock risk.

Tools Needed

Suggested Reading