Hack Your Roshamglo Badge

≡ Pages
Contributors: Shawn Hymel

Install USB Driver

Roshamglo is emulating USB 1.1 using two of its pins. However, there are no common operating system drivers available that work with this custom USB class. As a result, we will need to install custom drivers in order to communicate with (and send our Arduino programs to) the Roshamglo board. Choose your operating system below and follow the directions to install the driver.

Note: We did not write the USB firmware nor the driver. We simply modified them to work with Roshamglo. The true geniuses are the fine folks who wrote micronucleus and libusb.

Windows

Make sure the Roshamglo board is OFF, hold the Down button (pull the five-way switch toward the SparkFun logo) and insert it into an available USB slot.

Plug Roshamglo into a USB slot

Once plugged in, the status LED should begin to quickly flash red in short bursts. This means the badge is in "Bootloader Mode."

Flashing LED means it's in bootloader mode

Download the SparkFun ATtiny USB drivers by clicking on the link below.

Unzip the file. Open the Windows Device Manager, and you should see an Unknown device. Right-click on Unknown device and select Update Driver Software.

Updating driver for Roshamglo

In the pop-up window, click Browse my computer for driver software.

Search for SparkFun USB drivers

Click Browse... and open the folder that contains the drivers you just unzipped. It will likely be the sparkfun_attiny_usb_driver folder.

Installing the USB drivers

Click Next. You may get a warning pop-up that says "Windows can't verify the publisher of this driver software." That's OK. Just click Install the driver software anyway.

Tell Windows we want to install the driver software anyway

You should see a notification that the SparkFun ATtiny driver was installed successfully. Close that window, and verify that your Unknown device now shows up as SparkFun ATtiny in the Device Manager.

Successful installation of the SparkFun ATtiny USB driver

MacOS

You'll need to install Homebrew and use it to install libusb. Enter the following commands into a Terminal:

/usr/bin/ruby -e "$(curl -fsSL https://raw.githubusercontent.com/Homebrew/install/master/install)"
brew doctor
brew install libusb-compat

Linux

Good news! Linux doesn't require special drivers. However, you will need to do one of the following to be able to program Roshamglo from Arduino:

1) When you download the Arduino IDE (next section), make sure you run it as root: sudo ./arduino

Running Arduino as root

2) Or, you can add some udev rules so that Linux enumerates your device with write permissions. Create a file in rules.d:

sudo edit /etc/udev/rules.d/49-micronucleus.rules

Copy the following contents into that file:

# UDEV Rules for Micronucleus boards including the Digispark.
# This file must be placed at:
#
# /etc/udev/rules.d/49-micronucleus.rules    (preferred location)
#   or
# /lib/udev/rules.d/49-micronucleus.rules    (req'd on some broken systems)
#
# After this file is copied, physically unplug and reconnect the board.
#
SUBSYSTEMS=="usb", ATTRS{idVendor}=="16d0", ATTRS{idProduct}=="0753", MODE:="0666"
KERNEL=="ttyACM*", ATTRS{idVendor}=="16d0", ATTRS{idProduct}=="0753", MODE:="0666", ENV{ID_MM_DEVICE_IGNORE}="1"
#
# If you share your linux system with other users, or just don't like the
# idea of write permission for everybody, you can replace MODE:="0666" with
# OWNER:="yourusername" to create the device owned by you, or with
# GROUP:="somegroupname" and mange access using standard unix groups.

Save and exit.