Flex Sensor Hookup Guide

≡ Pages
Contributors: jimblom, bboyho

Example Program

Here is a simple Arduino example based on the circuit above. Copy and paste this into your Arduino IDE, then upload!

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

If you have not previously installed an Arduino library, please check out our installation guide.

language:c
/******************************************************************************
Flex_Sensor_Example.ino
Example sketch for SparkFun's flex sensors
  (https://www.sparkfun.com/products/10264)
Jim Lindblom @ SparkFun Electronics
April 28, 2016

Create a voltage divider circuit combining a flex sensor with a 47k resistor.
- The resistor should connect from A0 to GND.
- The flex sensor should connect from A0 to 3.3V
As the resistance of the flex sensor increases (meaning it's being bent), the
voltage at A0 should decrease.

Development environment specifics:
Arduino 1.6.7
******************************************************************************/
const int FLEX_PIN = A0; // Pin connected to voltage divider output

// Measure the voltage at 5V and the actual resistance of your
// 47k resistor, and enter them below:
const float VCC = 4.98; // Measured voltage of Ardunio 5V line
const float R_DIV = 47500.0; // Measured resistance of 3.3k resistor

// Upload the code, then try to adjust these values to more
// accurately calculate bend degree.
const float STRAIGHT_RESISTANCE = 37300.0; // resistance when straight
const float BEND_RESISTANCE = 90000.0; // resistance at 90 deg

void setup() 
{
  Serial.begin(9600);
  pinMode(FLEX_PIN, INPUT);
}

void loop() 
{
  // Read the ADC, and calculate voltage and resistance from it
  int flexADC = analogRead(FLEX_PIN);
  float flexV = flexADC * VCC / 1023.0;
  float flexR = R_DIV * (VCC / flexV - 1.0);
  Serial.println("Resistance: " + String(flexR) + " ohms");

  // Use the calculated resistance to estimate the sensor's
  // bend angle:
  float angle = map(flexR, STRAIGHT_RESISTANCE, BEND_RESISTANCE,
                   0, 90.0);
  Serial.println("Bend: " + String(angle) + " degrees");
  Serial.println();

  delay(500);
}

After uploading, open your serial monitor, and set the baud rate to 9600 bps.

If you bend the flex sensor, you should see resistance and estimated angle calculations change:

flex sensor readings to serial monitor

If the value's don't seem correct, make sure the constants VCC and, more importantly, R_DIV are accurate. If you used something other than a 47kΩ resistor, enter that value in for R_DIV.

Through trial-and-error, try to hone in on more accurate values for STRAIGHT_RESISTANCE and BEND_RESISTANCE -- your flex sensor's resistance when it's straight and bent at 90°.