Dot/Bar Display Driver Hookup Guide

≡ Pages
Contributors: jimblom

IC Overview

On this page we'll take a look at the pinout of the 18-pin LM3914/6. We'll also dig a little deeper to see what makes the ICs do what they do.

The Pinout

The DIP (through-hole, dual-inline package) version of this chip has 18 pins, and both a dot and notch to indicate polarity.

Chip pinout

Over half of the pins are in charge of driving the LEDs. The remaining pins are used for power, reference voltages, and control of the IC. Here is an overview of the chip's pinout:

Pin #Pin NamePin FunctionPin #Pin NamePin Function
1LED 1First (lowest value) LED18LED 22nd LED
2V−Ground17LED 33rd LED
3V+Supply voltage (3-25V)16LED 44th LED
4RLODivider low voltage15LED 55th LED
5Signal InAnalog signal in14LED 66th LED
6RHIDivider high voltage13LED 77th LED
7Ref OutReference output voltage12LED 88th LED
8Ref AdjVoltage reference adjust11LED 99th LED
9ModeDot/Bar mode select10LED 10Last (higest analog input) LED

That may seem a daunting list of pins and reference voltages to supply, but in reality it can be very simple. Many of those pins can either be tied to ground, VCC, or even left floating. Other pins may require a resistor or two to set constant current or voltage values.

LED Outputs

The LED outputs are all open-collectors, so they sink current. Connect the cathode of an LED to these pins and tie the other pin of the LED -- the anode -- to your voltage supply. There is no need for current limiting resistors, as the chip takes care of current regulation.

Mode Select

The Mode pin allows you to select between "bar" mode and "dot" mode. In bar mode, all LEDs sequentially turn on. So, if the signal voltage is near max, all LEDs should be on. In "dot" mode just a single LED is on at any time. Connect mode directly to the power source for bar mode, and leave it floating for dot mode.

ModeMode Pin Setting
Bar GraphTied directly to V+
Dot DisplayLeft floating (no connection)
Dot Display (cascaded drivers)Mode pin of first driver connected to pin 1 of next.

Setting the Analog Range with RHI and RLO

The RHI (pin 6) and RLO (pin 4) pins are used to map the sensing range of the LM3914/6. RHI sets the maximum voltage, and RLO sets the minimum voltage.

These two pins can be connected to any voltage as long as it's 1.5V below the supply voltage (V+), and greater than 0V.

Setting LED Current with Ref Out

The current drawn out of the Ref Out pin (pin 7) sets the current that flows through each LED, so this pin can be used to adjust the LED brightness.

If a resistor (RL) is connected from that pin to ground, the current flowing through each LED will be about equal to this equation:

LED current equation

So, for example, if you have a 1kΩ resistor connected from pin 7 to ground, the LED current should be around 12.5 mA.

If you have a more complex circuit connected to this pin, remember that the voltage between Ref Out and Ref Adj pin (pin 8) should be 1.25V. And the LED current is equal to 10 times the current coming out of Ref Out.

The Internals -- A Chain of Comparators

Note: It's not critical to understand how these chips work, but it is a neat study into the internals of an integrated circuit. Feel free to skip to the next page, if this looks a little too much like a Circuits I class.

The image below, from the LM3914/6 datasheet, provides an excellent overview of what's going on inside these chips:

LM3914/6 Block Diagram

Each LED is controlled by the output of a comparator, which is a very simple op amp circuit. If the voltage going into the + (non-inverting) pin is greater than that going into − (inverting), the comparator outputs a 1 (high, or, in this case the pin "floats"). If the − pin voltage is greater than +, the output of the comparator is a 0 (pulled towards ground).

Comparator input/output equation

The input/output combinations of a comparator.

Inside the chip, the analog control signal from pin 5 is connected to each of the inverting (−) inputs on the comparators. The non-inverting (+) inputs of the comparators are connected to a string of 1kΩ resistors, which create larger-and-larger voltage dividers. The + voltage on the first comparator will be the divider input voltage (RHI − RLO), while the + voltage on the last comparator is 1/10th of that voltage.

To turn an LED on -- meaning the comparator's output is 0 -- the analog signal voltage must be greater than the divided input on a comparator. So a smaller signal voltage is required to turn on the first LED in comparison to any of the following.

Voltage and Current Ratings

The LM3914/6 ICs have a very wide supply voltage range: anywhere from 1.8V to 18V.

The voltage between the RHI and RLO pins can be anything between 0V (thought, that wouldn't be too useful) and 1.5V below the supply voltage. So, if you're powering the chip at 5V, it'll only be able to map voltages between 0V and 3.5V.

Also, keep in mind the current that might be flowing through the chip. Each LED can take anywhere between 7 and 13 mA, and to supply the chip you'll need an additional 2 to 9 mA.