Capacitive Touch Slider (CAP1203) Hookup Guide

≡ Pages
Contributors: andreadevo

Hardware Overview

Note: If you want to do anything outside of what is covered in this tutorial or the example code, please refer to the CAP1203 datasheet for exact details on the sensor functionality.

Power

You can provide 3.3V through the polarized Qwiic connectors on the board or through the 3V3 labeled pin on the through-hole header. The Qwiic system is meant to use 3.3V, so be sure you are NOT using another voltage when using the Qwiic system. When you have correctly powered the board, the red power LED will turn on.

Power LED and Breakout Pin

Power LED, Breakout Pin, and Qwiic Connectors

Qwiic Connectors or I2C Pins

There are two Qwiic connectors on the back of the board to easily connect the sensor to I2C. If you prefer the old school method of connecting to I2C, we've also included four breakout pins on the side of the board.

Qwiic Connectors and I2C pins

Qwiic Connectors and I2C Breakout Pins

Interrupt Pin and LED

The interrupt pin is an active low output which is triggered each each time a sensor pad is touched. You can connect to this pin if you want to check when an interrupt occurs. On the front side of the board, the green LED in the bottom right corner also signals when an interrupt occurs.

Interrupt Breakout Pin

Interrupt Breakout Pin

Interrupt LED
Interrupt LED

Capacitive Touch Pads and Pins

On the front of the board, there is an arrow shape which contains three separate capacitive touch pads. In order to know which pad is which, orient the board with the arrow pointing in the right direction. We will reference these capacitive touch pads as the left pad, the middle pad, and the right pad throughout the guide and in the code. We also broke out the capacitive touch sensor lines as plated through-holes on the top of the board. You can use these pins to connect to your own capacitive touch pads. The CS1 pin connects to the left pad, the CS2 pin connects to the middle pad, and the CS3 pin connects to the right pad.

Left Pad Highlighted
Middle Pad Highlighted
Right Pad Highlighted

Left, Middle, and Right Touch Pads

Capacitive Touch Pads Breakout Pins

Capacitive Touch Pad Breakout Pins

Jumpers

There are 3 jumper pads on the back of the board, each labeled with its function. First, on upper left side of the board, there is a two way jumper labeled INT that connects to a 10kΩ pull-up resistor on the interrupt data line. If you cut this jumper, it will disconnect the 10kkΩ pull-up resistor from the interrupt data line. Next, on the lower left side of the board, there is a two way jumper labeled LED that connects to the green interrupt LED. If you cut this jumper, it will disconnect the LED from the interrupt line, effectively disabling the green LED's functionality. Lastly, on the lower half of the board, there is a three way jumper labeled I²C that connects two 2.2kkΩ pull-up resistors to the I2C data lines. If you have multiple devices on your I2C data lines, then you may consider cutting this jumper. Not sure how to cut a jumper? Read here!

Jumper Pads

Jumper pads for the INT pin pull-up, LED disable, and I2C pullup

Board Measurements

The SparkFun Capacitive Touch measures 1 inch by 1.5 inches.

Board Measurements