AST-CAN485 Hookup Guide

≡ Pages
Contributors: JamesBM

Companion Boards

If you are looking to control 24V inputs and outputs using the CAN485, check out the I/O shield (24V) for wired connections.

AST-CAN485 I/O Shield (24V) Hookup Guide

February 14, 2019
The AST-CAN485 I/O Shield is an Arduino shield that will allow the user to interface the AST-CAN485 Dev Board with 24V inputs and outputs, which expands its usefulness into industrial systems.

If you need to control RS485 or CAN devices remotely, check out the WiFi shield..

AST-CAN485 WiFi Shield Hookup Guide

February 14, 2019
Hookup Guide for the AST-CAN485 WiFi Shield.