Artemis Development with Arduino

≡ Pages
Contributors: Nate, Ell C

Example: All the Features

We've built the Arduino core for Artemis from the ground up. Be sure to checkout the large number of built-in examples. You'll find them under File->Examples->'Examples for Artemis'.

Arduino sub menu showing Artemis examples

Click above image for full menu context

We've got examples for setting up multiple I2C ports (it's amazingly easy), writing to EEPROM, using SoftwareSerial (all 48 pins can be serial!), using the the onboard microphone, and using servos (up to 32!). We're adding more all the time so be sure to keep your core up to date.