APDS-9960 RGB and Gesture Sensor Hookup Guide

≡ Pages
Contributors: Shawn Hymel

Board Overview

Pin Descriptions

The APDS-9960 breakout board provides 6 pins to provide power to the sensor and I2C bus.

Front of APDS-9960 breakout board

Pin LabelDescription
VLOptional power to the IR LED if PS jumper is disconnected. Must be 3.0 - 4.5V
GNDConnect to ground.
VCCUsed to power the APDS-9960 sensor. Must be 2.4 - 3.6V
SDAI2C data
SCLI2C clock
INTExternal interrupt pin. Active LOW on interrupt event


Setting the Jumpers

On the front of the breakout board are 2 solder jumpers:

  • PS -- This jumper connects the power supplies of the sensor and IR LED (also located on the APDS-9960) together. When the jumper is closed (i.e. connected), you only need to supply power to the VCC pin to power both the sensor and the IR LED. If the jumper is open, you need to provide power to both the VCC (2.4 - 3.6V) and VL (3.0 - 4.5V) pins separately. This jumper is closed by default.
  • I2C PU -- This is a 3-way solder jumper that is used to connect and disconnect the I2C pullup resistors. By default, this jumper is closed, which means that both SDA and SCL lines have connected pullup resistors on the breakout board. Use some solder wick to open the jumper if you do not need the pullup resistors (e.g. you have pullup resistors that are located on the I2C bus somewhere else).