What is a Battery?

≡ Pages
Contributors: Shawn Hymel

Introduction

Batteries are a collection of one or more cells whose chemical reactions create a flow of electrons in a circuit. All batteries are made up of three basic components: an anode (the '-' side), a cathode (the '+' side), and some kind of electrolyte (a substance that chemically reacts with the anode and cathode).

When the anode and cathode of a battery is connected to a circuit, a chemical reaction takes place between the anode and the electrolyte. This reaction causes electrons to flow through the circuit and back into the cathode where another chemical reaction takes place. When the material in the cathode or anode is consumed or no longer able to be used in the reaction, the battery is unable to produce electricity. At that point, your battery is "dead."

Batteries that must be thrown away after use are known as primary batteries. Batteries that can be recharged are called secondary batteries.

Charging a LiPo

Lithium polymer batteries, for example, can be recharged

Without batteries, your quadcopter would have to be tethered to the wall, you would have to hand crank your car, and your Xbox controller would have to plugged in all the time (like in the good old days). Batteries offer a way to store electrical potential energy in a portable container.

Various batteries

Batteries come in a variety of shapes, sizes, and chemistries.

The invention of the modern battery is often attributed to Alessandro Volta. It actually started with a surprising accident involving the dissection of a frog.

What You Will Learn

The following topics will be covered in detail in this tutorial:

  • How batteries were invented
  • What parts make up a battery
  • How a battery works
  • Common terms used to describe batteries
  • Various ways to use batteries in circuits

Suggested Reading

There are a few concepts that you might want to be familiar with before starting to read this guide:


Looking to explore different batteries?

We've got you covered!

Lithium Ion Battery - 400mAh

PRT-13851
$7.98

Lithium Ion Battery - 18650 Cell (2600mAh)

PRT-12895
$9.83

Coin Cell Battery - 20mm (CR2032)

PRT-00338
$2.25

9V Alkaline Battery

PRT-10218
$2.50